BITPlatform Common
Macros | |
#define | SL_CLEAR_BIT(val, mask) ((val) = ((val) & (~(mask)))) |
Clear specified bit(s) in a value. | |
#define | SL_IS_ANY_BIT_CLEAR(val, mask) ((((val) & (mask)) == (mask)) ? (false) : (true)) |
Determine if any specified bit(s) in a value are clear. | |
#define | SL_IS_ANY_BIT_SET(val, mask) ((((val) & (mask)) == 0u) ? (false) : (true)) |
Determine if any specified bit(s) in a value are set. | |
#define | SL_IS_BIT_CLEAR(val, mask) (((((val) & (mask)) == 0u) && ((mask) != 0u)) ? (true) : (false)) |
Determine if specified bit(s) in a value are clear. | |
#define | SL_IS_BIT_SET(val, mask) (((((val) & (mask)) == (mask)) && ((mask) != 0u)) ? (true) : (false)) |
Determine if specified bit(s) in a value are set. | |
#define | SL_SET_BIT(val, mask) ((val) = ((val) | (mask))) |
Set specified bit(s) in a value. | |
Macro Definition Documentation
#define SL_CLEAR_BIT | ( | val, |
|
mask |
|||
) | ((val) = ((val) & (~(mask)))) |
Clear specified bit(s) in a value.
- Parameters
-
val
Value to modify by clearing specified bit(s). mask
Mask of bits to clear.
- Returns
- Modified value with specified bit(s) clear.
- Note
- 'val' & 'mask' SHOULD be unsigned integers.
- 'mask' SHOULD be cast with the same data type than 'val'.
Definition at line 63
of file sl_bit.h
.
#define SL_IS_ANY_BIT_CLEAR | ( | val, |
|
mask |
|||
) | ((((val) & (mask)) == (mask)) ? (false) : (true)) |
Determine if any specified bit(s) in a value are clear.
- Parameters
-
val
Value to check for specified bit(s) clear. mask
Mask of bits to check if clear (see Note #2).
- Returns
- true, if ANY specified bit(s) are clear in value.
false, if ALL specified bit(s) are NOT clear in value.
- Note
- 'val' & 'mask' SHOULD be unsigned integers.
- NULL 'mask' allowed; returns 'false' since NO mask bits specified.
Definition at line 142
of file sl_bit.h
.
#define SL_IS_ANY_BIT_SET | ( | val, |
|
mask |
|||
) | ((((val) & (mask)) == 0u) ? (false) : (true)) |
Determine if any specified bit(s) in a value are set.
- Parameters
-
val
Value to check for specified bit(s) set. mask
Mask of bits to check if set (see Note #2).
- Returns
- true, if ANY specified bit(s) are set in value.
false, if ALL specified bit(s) are NOT set in value.
- Note
- 'val' & 'mask' SHOULD be unsigned integers.
- NULL 'mask' allowed; returns 'false' since NO mask bits specified.
Definition at line 122
of file sl_bit.h
.
#define SL_IS_BIT_CLEAR | ( | val, |
|
mask |
|||
) | (((((val) & (mask)) == 0u) && ((mask) != 0u)) ? (true) : (false)) |
Determine if specified bit(s) in a value are clear.
- Parameters
-
val
Value to check for specified bit(s) clear. mask
Mask of bits to check if clear.
- Returns
- true, if ALL specified bit(s) are clear in value.
false, if ALL specified bit(s) are NOT clear in value.
- Note
- val' & 'mask' SHOULD be unsigned integers.
- NULL 'mask' allowed; returns 'false' since NO mask bits specified.
Definition at line 102
of file sl_bit.h
.
#define SL_IS_BIT_SET | ( | val, |
|
mask |
|||
) | (((((val) & (mask)) == (mask)) && ((mask) != 0u)) ? (true) : (false)) |
Determine if specified bit(s) in a value are set.
- Parameters
-
val
Value to check for specified bit(s) set. mask
Mask of bits to check if set.
- Returns
- true, if ALL specified bit(s) are set in value.
false, if ALL specified bit(s) are NOT set in value.
- Note
- 'val' & 'mask' SHOULD be unsigned integers.
- NULL 'mask' allowed; returns 'false' since NO mask bits specified.
Definition at line 83
of file sl_bit.h
.
#define SL_SET_BIT | ( | val, |
|
mask |
|||
) | ((val) = ((val) | (mask))) |
Set specified bit(s) in a value.
- Parameters
-
val
Value to modify by setting specified bit(s). mask
Mask of bits to set.
- Returns
- Modified value with specified bit(s) set.
- Note
- 'val' & 'mask' SHOULD be unsigned integers.
Definition at line 45
of file sl_bit.h
.