Direct_Transmit_PluginEMDRV > EZRADIODRV > Plugin_System

Detailed Description

Direct transmit plugin, see Plugin System Layer for detailed documentation.


     

.

Data Structures

struct EZRADIODRV_DirectTxHandle
EzRadio direct tx plug-in instance initialization and handler structure.

Macros

#define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT
Configuration data for EzRadio direct tx plug-in.

Typedefs

typedef struct EZRADIODRV_DirectTxHandle EZRADIODRV_DirectTxHandle_t
EzRadio direct tx plug-in instance initialization and handler structure.

Functions

Ecode_t ezradioStartDirectTransmit ( EZRADIODRV_Handle_t radioHandle)
Starts direct transmission with the radio configurations from the radioHandle parameter.
Ecode_t ezradioStopDirectTransmit (void)
Stops direct transmission.

Macro Definition Documentation

#define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT
Value:
{ /* PN9 */ \
0, /* Channel */ \
},

Configuration data for EzRadio direct tx plug-in.

Definition at line 71 of file ezradio_direct_transmit_plugin.h .

Function Documentation

Ecode_t ezradioStartDirectTransmit ( EZRADIODRV_Handle_t radioHandle )

Starts direct transmission with the radio configurations from the radioHandle parameter.

Parameters
radioHandle Handler of the EzRadio driver instance where channel configuration is set.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 54 of file ezradio_direct_transmit_plugin.c .

References EZRADIODRV_DirectTxHandle::channel , EZRADIODRV_HandleData::directTx , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED , ezradio_get_int_status() , ezradio_request_device_state() , and ezradio_start_tx() .

Ecode_t ezradioStopDirectTransmit ( void )

Stops direct transmission.

Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 85 of file ezradio_direct_transmit_plugin.c .

References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .