__BAP_Config Struct ReferenceBSP > Thunderboard Sense BSP > BAP - Barometric Pressure Sensor
Structure to configure the BMP280 device.
Definition at line 59
of file bap.h
.
#include <
bap.h
>
Data Fields | |
uint8_t | oversampling |
uint8_t | powerMode |
uint8_t | standbyTime |
Field Documentation
uint8_t __BAP_Config::oversampling |
uint8_t __BAP_Config::powerMode |
SLEEP, FORCED or NORMAL power mode setting
Definition at line 61
of file bap.h
.
Referenced by BAP_config().
uint8_t __BAP_Config::standbyTime |
The documentation for this struct was generated from the following file:
- C:/repos/super/hardware/kit/common/bsp/thunderboard/
bap.h