TempSensorKit Drivers
Detailed Description
Driver for DS75 I2C temperature sensor.
Data Structures | |
struct | TEMPSENS_Temp_TypeDef |
Macros | |
#define | TEMPSENS_DK_ADDR 0x90 |
Enumerations | |
enum | TEMPSENS_Register_TypeDef { tempsensRegTemp = 0, tempsensRegConfig = 1, tempsensRegHysteresis = 2, tempsensRegShutdown = 3 } |
Functions | |
void | TEMPSENS_Celsius2Fahrenheit (TEMPSENS_Temp_TypeDef *temp) |
Convert temperature from Celsius to Fahrenheit. | |
int | TEMPSENS_RegisterGet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t *val) |
Read sensor register content. | |
int | TEMPSENS_RegisterSet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Register_TypeDef reg, uint16_t val) |
Write to sensor register. | |
int | TEMPSENS_TemperatureGet (I2C_TypeDef *i2c, uint8_t addr, TEMPSENS_Temp_TypeDef *temp) |
Fetch current temperature from temperature sensor (in Celsius). | |
Macro Definition Documentation
#define TEMPSENS_DK_ADDR 0x90 |
I2C device address for temperature sensor on EFM32GG/LG/WG DK
Definition at line 55
of file tempsens.h
.
Enumeration Type Documentation
Function Documentation
void TEMPSENS_Celsius2Fahrenheit | ( | TEMPSENS_Temp_TypeDef * | temp | ) |
Convert temperature from Celsius to Fahrenheit.
- Parameters
-
[in,out] temp
Reference to structure to holding temperature in Celsius to convert. Upon return, it has been changed to Fahrenheit.
Definition at line 58
of file tempsens.c
.
References TEMPSENS_Temp_TypeDef::f, and TEMPSENS_Temp_TypeDef::i.
int TEMPSENS_RegisterGet | ( | I2C_TypeDef * | i2c, |
uint8_t | addr, |
||
TEMPSENS_Register_TypeDef | reg, |
||
uint16_t * | val |
||
) |
Read sensor register content.
If reading the temperature register, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] reg
Register to read. [out] val
Reference to place register read.
- Returns
- Returns 0 if register read, <0 if unable to read register.
Definition at line 99
of file tempsens.c
.
References I2C_TransferSeq_TypeDef::addr, I2C_TransferSeq_TypeDef::buf, I2C_TransferSeq_TypeDef::data, I2C_TransferSeq_TypeDef::flags, I2C_FLAG_WRITE_READ, I2CSPM_Transfer(), i2cTransferDone, I2C_TransferSeq_TypeDef::len, and tempsensRegConfig.
Referenced by TEMPSENS_TemperatureGet().
int TEMPSENS_RegisterSet | ( | I2C_TypeDef * | i2c, |
uint8_t | addr, |
||
TEMPSENS_Register_TypeDef | reg, |
||
uint16_t | val |
||
) |
Write to sensor register.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [in] reg
Register to write (temperature register cannot be written). [in] val
Value used when writing to register.
- Returns
- Returns 0 if register written, <0 if unable to write to register.
Definition at line 156
of file tempsens.c
.
References I2C_TransferSeq_TypeDef::addr, I2C_TransferSeq_TypeDef::buf, I2C_TransferSeq_TypeDef::data, I2C_TransferSeq_TypeDef::flags, I2C_FLAG_WRITE, I2CSPM_Transfer(), i2cTransferDone, I2C_TransferSeq_TypeDef::len, tempsensRegConfig, and tempsensRegTemp.
int TEMPSENS_TemperatureGet | ( | I2C_TypeDef * | i2c, |
uint8_t | addr, |
||
TEMPSENS_Temp_TypeDef * | temp |
||
) |
Fetch current temperature from temperature sensor (in Celsius).
If reading the temperature, when a measurement is completed inside the sensor device, the new measurement may not be stored. For this reason, the temperature should not be polled with a higher frequency than the measurement conversion time for a given resolution configuration. Please refer to sensor device datasheet.
- Note
- The sensor on the the DK, STDS75, does not seem to have any check on max temperature limit, ie when exceeding specified max 125 C limit, it will keep increasing 9 bit counter to max representable 9 bit value of 127.5 C and then flip over to negative numbers. There is no limit check in this implementation on such issues.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for temperature sensor, in 8 bit format, where LSB is reserved for R/W bit. [out] temp
Reference to structure to place temperature (in Celsius).
- Returns
- Returns 0 if temperature read, <0 if unable to read temperature.
Definition at line 223
of file tempsens.c
.
References TEMPSENS_Temp_TypeDef::f, TEMPSENS_Temp_TypeDef::i, TEMPSENS_RegisterGet(), and tempsensRegTemp.