MSC_EccConfig_TypeDef Struct ReferenceEMLIB > MSC
ECC configuration.
Definition at line
237
of file
em_msc.h
.
#include <
em_msc.h
>
Data Fields |
|
| uint32_t | dmaChannels [2] |
| bool | enableEccBank [ MSC_ECC_BANKS ] |
Field Documentation
| uint32_t MSC_EccConfig_TypeDef::dmaChannels[2] |
Array of 2 DMA channel numbers to use for ECC initialization.
Definition at line
242
of file
em_msc.h
.
Referenced by MSC_EccConfigSet() .
| bool MSC_EccConfig_TypeDef::enableEccBank[ MSC_ECC_BANKS ] |
Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.
Definition at line
238
of file
em_msc.h
.
Referenced by MSC_EccConfigSet() .
The documentation for this struct was generated from the following file:
-
C:/repos/super/platform/emlib/inc/
em_msc.h