BURTC_Init_TypeDef Struct ReferenceEMLIB > BURTC
BURTC initialization structure for Series 2 devices.
Definition at line
145
of file
em_burtc.h
.
#include <
em_burtc.h
>
Data Fields |
|
| uint32_t | clkDiv |
| bool | compare0Top |
| bool | debugRun |
| bool | em4comp |
| bool | em4overflow |
| bool | start |
Field Documentation
| uint32_t BURTC_Init_TypeDef::clkDiv |
Clock divider. Supported range is 1-32768
Definition at line
148
of file
em_burtc.h
.
Referenced by BURTC_Init() .
| bool BURTC_Init_TypeDef::compare0Top |
Set if Compare Value 0 is also top value (counter restart)
Definition at line
149
of file
em_burtc.h
.
Referenced by BURTC_Init() .
| bool BURTC_Init_TypeDef::debugRun |
If true, counter will keep running under debug halt
Definition at line
147
of file
em_burtc.h
.
Referenced by BURTC_Init() .
| bool BURTC_Init_TypeDef::em4comp |
Enable EM4 wakeup on compare match.
Definition at line
150
of file
em_burtc.h
.
Referenced by BURTC_Init() .
| bool BURTC_Init_TypeDef::em4overflow |
Enable EM4 wakeup on counter overflow.
Definition at line
151
of file
em_burtc.h
.
Referenced by BURTC_Init() .
| bool BURTC_Init_TypeDef::start |
Start BURTC after initialization
Definition at line
146
of file
em_burtc.h
.
Referenced by BURTC_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/super/platform/emlib/inc/
em_burtc.h