LDMA_Descriptor_t Union ReferenceEMLIB > LDMA
DMA descriptor.
The LDMA DMA controller supports three different DMA descriptors. Each consists of four WORDs which map directly onto HW control registers for a given DMA channel. The three descriptor types are XFER, SYNC and WRI. Refer to the reference manual for further information.
Definition at line 787
of file em_ldma.h
.
#include <
em_ldma.h
>
Data Fields | |
struct { | |
uint32_t blockSize: 4 | |
uint32_t byteSwap: 1 | |
uint32_t decLoopCnt: 1 | |
uint32_t doneIfs: 1 | |
uint32_t dstAddrMode: 1 | |
uint32_t dstInc: 2 | |
uint32_t ignoreSrec: 1 | |
uint32_t link: 1 | |
int32_t linkAddr: 30 | |
uint32_t linkMode: 1 | |
uint32_t matchEn: 8 | |
uint32_t matchVal: 8 | |
uint32_t reqMode: 1 | |
uint32_t reserved0: 1 | |
uint32_t reserved3: 16 | |
uint32_t reserved4: 16 | |
uint32_t size: 2 | |
uint32_t srcAddrMode: 1 | |
uint32_t srcInc: 2 | |
uint32_t structReq: 1 | |
uint32_t structType: 2 | |
uint32_t syncClr: 8 | |
uint32_t syncSet: 8 | |
uint32_t xferCnt: 11 | |
} | sync |
struct { | |
uint32_t blockSize: 4 | |
uint32_t byteSwap: 1 | |
uint32_t decLoopCnt: 1 | |
uint32_t doneIfs: 1 | |
uint32_t dstAddr | |
uint32_t dstAddrMode: 1 | |
uint32_t dstInc: 2 | |
uint32_t ignoreSrec: 1 | |
uint32_t immVal | |
uint32_t link: 1 | |
int32_t linkAddr: 30 | |
uint32_t linkMode: 1 | |
uint32_t reqMode: 1 | |
uint32_t reserved0: 1 | |
uint32_t size: 2 | |
uint32_t srcAddrMode: 1 | |
uint32_t srcInc: 2 | |
uint32_t structReq: 1 | |
uint32_t structType: 2 | |
uint32_t xferCnt: 11 | |
} | wri |
struct { | |
uint32_t blockSize: 4 | |
uint32_t byteSwap: 1 | |
uint32_t decLoopCnt: 1 | |
uint32_t doneIfs: 1 | |
uint32_t dstAddr | |
uint32_t dstAddrMode: 1 | |
uint32_t dstInc: 2 | |
uint32_t ignoreSrec: 1 | |
uint32_t link: 1 | |
int32_t linkAddr: 30 | |
uint32_t linkMode: 1 | |
uint32_t reqMode: 1 | |
uint32_t reserved0: 1 | |
uint32_t size: 2 | |
uint32_t srcAddr | |
uint32_t srcAddrMode: 1 | |
uint32_t srcInc: 2 | |
uint32_t structReq: 1 | |
uint32_t structType: 2 | |
uint32_t xferCnt: 11 | |
} | xfer |
Field Documentation
uint32_t LDMA_Descriptor_t::blockSize |
Number of unit transfers per arbitration cycle.
Definition at line 798
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::byteSwap |
Enable byte swapping transfers.
Definition at line 797
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::decLoopCnt |
Enable looped transfers.
Definition at line 801
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::doneIfs |
Generate interrupt when done.
Definition at line 799
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::dstAddr |
DMA destination address.
DMA write destination address.
Definition at line 810
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::dstAddrMode |
Destination addressing mode.
Definition at line 807
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::dstInc |
Destination address increment unit size.
Definition at line 805
of file em_ldma.h
.
Referenced by MIC_init().
uint32_t LDMA_Descriptor_t::ignoreSrec |
Ignore single requests.
Definition at line 802
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::immVal |
Data to be written at dstAddr.
Definition at line 867
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::link |
Enable LINKLOAD when transfer is done.
Definition at line 813
of file em_ldma.h
.
int32_t LDMA_Descriptor_t::linkAddr |
Address of next (linked) descriptor.
Definition at line 814
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::linkMode |
Select absolute or relative link address.
Definition at line 812
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::matchEn |
Sync trigger match enable.
Definition at line 841
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::matchVal |
Sync trigger match value.
Definition at line 840
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::reqMode |
Block or cycle transfer selector.
Definition at line 800
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::size |
uint32_t LDMA_Descriptor_t::srcAddr |
DMA source address.
Definition at line 809
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::srcAddrMode |
Source addressing mode.
Definition at line 806
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::srcInc |
Source address increment unit size.
Definition at line 803
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::structReq |
DMA transfer trigger during LINKLOAD.
Definition at line 795
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::structType |
Set to 0 to select XFER descriptor type.
Set to 1 to select SYNC descriptor type.
Set to 2 to select WRITE descriptor type.
Definition at line 793
of file em_ldma.h
.
struct { ... } LDMA_Descriptor_t::sync |
SYNCHRONIZE DMA descriptor, used for intra channel transfer synchronization.
uint32_t LDMA_Descriptor_t::syncClr |
Clear bits in LDMA_CTRL.SYNCTRIG register.
Definition at line 838
of file em_ldma.h
.
uint32_t LDMA_Descriptor_t::syncSet |
Set bits in LDMA_CTRL.SYNCTRIG register.
Definition at line 837
of file em_ldma.h
.
struct { ... } LDMA_Descriptor_t::wri |
WRITE DMA descriptor, used for write immediate operations.
struct { ... } LDMA_Descriptor_t::xfer |
TRANSFER DMA descriptor, this is the only descriptor type which can be used to start a DMA transfer.
Referenced by MIC_init().
uint32_t LDMA_Descriptor_t::xferCnt |
Transfer count minus one.
Definition at line 796
of file em_ldma.h
.
The documentation for this union was generated from the following file:
- C:/repos/super/platform/emlib/inc/
em_ldma.h