IADC_ScanTableEntry_t Struct ReferenceEMLIB > IADC
IADC scan table entry structure
Definition at line 765
of file em_iadc.h
.
#include <
em_iadc.h
>
Data Fields | |
bool | compare |
uint8_t | configId |
bool | includeInScan |
IADC_NegInput_t | negInput |
IADC_PosInput_t | posInput |
Field Documentation
bool IADC_ScanTableEntry_t::compare |
Perform digital window comparison on the result from this entry.
Definition at line 769
of file em_iadc.h
.
Referenced by IADC_initScan(), and IADC_updateScanEntry().
uint8_t IADC_ScanTableEntry_t::configId |
Configuration id.
Definition at line 768
of file em_iadc.h
.
Referenced by IADC_initScan(), and IADC_updateScanEntry().
bool IADC_ScanTableEntry_t::includeInScan |
Include this scan table entry in scan operation.
Definition at line 770
of file em_iadc.h
.
Referenced by IADC_initScan(), and IADC_updateScanEntry().
IADC_NegInput_t IADC_ScanTableEntry_t::negInput |
Port/pin input for the negative side of the ADC.
Definition at line 766
of file em_iadc.h
.
Referenced by IADC_initScan(), and IADC_updateScanEntry().
IADC_PosInput_t IADC_ScanTableEntry_t::posInput |
Port/pin input for the positive side of the ADC.
Definition at line 767
of file em_iadc.h
.
Referenced by IADC_initScan(), and IADC_updateScanEntry().
The documentation for this struct was generated from the following file:
- C:/repos/super/platform/emlib/inc/
em_iadc.h