LETIMEREMLIB
Detailed Description
Low Energy Timer (LETIMER) Peripheral API.
This module contains functions to control the LETIMER peripheral of Silicon Labs 32-bit MCUs and SoCs. The LETIMER is a down-counter that can keep track of time and output configurable waveforms.
Data Structures |
|
| struct | LETIMER_Init_TypeDef |
Macros |
|
| #define | LETIMER_INIT_DEFAULT |
Enumerations |
|
| enum |
LETIMER_RepeatMode_TypeDef
{
letimerRepeatFree = _LETIMER_CTRL_REPMODE_FREE, letimerRepeatOneshot = _LETIMER_CTRL_REPMODE_ONESHOT, letimerRepeatBuffered = _LETIMER_CTRL_REPMODE_BUFFERED, letimerRepeatDouble = _LETIMER_CTRL_REPMODE_DOUBLE } |
| enum |
LETIMER_UFOA_TypeDef
{
letimerUFOANone = _LETIMER_CTRL_UFOA0_NONE, letimerUFOAToggle = _LETIMER_CTRL_UFOA0_TOGGLE, letimerUFOAPulse = _LETIMER_CTRL_UFOA0_PULSE, letimerUFOAPwm = _LETIMER_CTRL_UFOA0_PWM } |
Functions |
|
| uint32_t | LETIMER_CompareGet (LETIMER_TypeDef *letimer, unsigned int comp) |
|
Get the LETIMER compare register value.
|
|
| void | LETIMER_CompareSet (LETIMER_TypeDef *letimer, unsigned int comp, uint32_t value) |
|
Set the LETIMER compare register value.
|
|
| uint32_t | LETIMER_CounterGet (LETIMER_TypeDef *letimer) |
|
Get LETIMER counter value.
|
|
| void | LETIMER_CounterSet (LETIMER_TypeDef *letimer, uint32_t value) |
|
Set LETIMER counter value.
|
|
| void | LETIMER_Enable (LETIMER_TypeDef *letimer, bool enable) |
|
Start/stop LETIMER.
|
|
| void | LETIMER_Init (LETIMER_TypeDef *letimer, const LETIMER_Init_TypeDef *init) |
|
Initialize LETIMER.
|
|
| __STATIC_INLINE void | LETIMER_IntClear (LETIMER_TypeDef *letimer, uint32_t flags) |
|
Clear one or more pending LETIMER interrupts.
|
|
| __STATIC_INLINE void | LETIMER_IntDisable (LETIMER_TypeDef *letimer, uint32_t flags) |
|
Disable one or more LETIMER interrupts.
|
|
| __STATIC_INLINE void | LETIMER_IntEnable (LETIMER_TypeDef *letimer, uint32_t flags) |
|
Enable one or more LETIMER interrupts.
|
|
| __STATIC_INLINE uint32_t | LETIMER_IntGet (LETIMER_TypeDef *letimer) |
|
Get pending LETIMER interrupt flags.
|
|
| __STATIC_INLINE uint32_t | LETIMER_IntGetEnabled (LETIMER_TypeDef *letimer) |
|
Get enabled and pending LETIMER interrupt flags.
|
|
| __STATIC_INLINE void | LETIMER_IntSet (LETIMER_TypeDef *letimer, uint32_t flags) |
|
Set one or more pending LETIMER interrupts from SW.
|
|
| uint32_t | LETIMER_RepeatGet (LETIMER_TypeDef *letimer, unsigned int rep) |
|
Get the LETIMER repeat register value.
|
|
| void | LETIMER_RepeatSet (LETIMER_TypeDef *letimer, unsigned int rep, uint32_t value) |
|
Set the LETIMER repeat counter register value.
|
|
| void | LETIMER_Reset (LETIMER_TypeDef *letimer) |
|
Reset LETIMER to the same state that it was in after a hardware reset.
|
|
| void | LETIMER_SyncWait (LETIMER_TypeDef *letimer) |
|
Wait for the LETIMER to complete all synchronization of register changes and commands.
|
|
| uint32_t | LETIMER_TopGet (LETIMER_TypeDef *letimer) |
|
Get the current LETIMER top value.
|
|
| void | LETIMER_TopSet (LETIMER_TypeDef *letimer, uint32_t value) |
|
Set the LETIMER top value.
|
|
Macro Definition Documentation
| #define LETIMER_INIT_DEFAULT |
Default configuration for LETIMER initialization structure.
Definition at line
126
of file
em_letimer.h
.
Referenced by MIC_init() .
Enumeration Type Documentation
Repeat mode.
Definition at line
57
of file
em_letimer.h
.
| enum LETIMER_UFOA_TypeDef |
Underflow action on output.
Definition at line
75
of file
em_letimer.h
.
Function Documentation
| uint32_t LETIMER_CompareGet | ( | LETIMER_TypeDef * |
letimer,
|
| unsigned int |
comp
|
||
| ) |
Get the LETIMER compare register value.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to get, either 0 or 1.
- Returns
- A compare register value, 0 if invalid register selected.
Definition at line
129
of file
em_letimer.c
.
| void LETIMER_CompareSet | ( | LETIMER_TypeDef * |
letimer,
|
| unsigned int |
comp,
|
||
| uint32_t |
value
|
||
| ) |
Set the LETIMER compare register value.
- Note
- The setting of a compare register requires synchronization into the low frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff).
Definition at line
218
of file
em_letimer.c
.
Referenced by LETIMER_TopSet() , and MIC_init() .
| uint32_t LETIMER_CounterGet | ( | LETIMER_TypeDef * |
letimer
|
) |
Get LETIMER counter value.
- Parameters
-
[in] letimerPointer to the LETIMER peripheral register block.
- Returns
- Current LETIMER counter value.
Definition at line
170
of file
em_letimer.c
.
| void LETIMER_CounterSet | ( | LETIMER_TypeDef * |
letimer,
|
| uint32_t |
value
|
||
| ) |
Set LETIMER counter value.
- Parameters
-
[in] letimerPointer to the LETIMER peripheral register block. [in] valueNew counter value.
Definition at line
189
of file
em_letimer.c
.
| void LETIMER_Enable | ( | LETIMER_TypeDef * |
letimer,
|
| bool |
enable
|
||
| ) |
Start/stop LETIMER.
- Note
- The enabling/disabling of the LETIMER modifies the LETIMER CMD register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block. [in] enableTrue to enable counting, false to disable.
Definition at line
272
of file
em_letimer.c
.
| void LETIMER_Init | ( | LETIMER_TypeDef * |
letimer,
|
| const LETIMER_Init_TypeDef * |
init
|
||
| ) |
Initialize LETIMER.
Note that the compare/repeat values must be set separately with LETIMER_CompareSet() and LETIMER_RepeatSet() . That should probably be done prior using this function if configuring the LETIMER to start when initialization is complete.
- Note
- The initialization of the LETIMER modifies the LETIMER CTRL/CMD registers which require synchronization into the low-frequency domain. If any of those registers are modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block. [in] initA pointer to the LETIMER initialization structure.
Definition at line
363
of file
em_letimer.c
.
References LETIMER_Init_TypeDef::bufTop , LETIMER_Init_TypeDef::comp0Top , LETIMER_Init_TypeDef::debugRun , LETIMER_Init_TypeDef::enable , LETIMER_Init_TypeDef::out0Pol , LETIMER_Init_TypeDef::out1Pol , LETIMER_Init_TypeDef::repMode , LETIMER_Init_TypeDef::topValue , LETIMER_Init_TypeDef::ufoa0 , and LETIMER_Init_TypeDef::ufoa1 .
Referenced by MIC_init() .
| __STATIC_INLINE void LETIMER_IntClear | ( | LETIMER_TypeDef * |
letimer,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending LETIMER interrupts.
- Parameters
-
[in] letimerPointer to LETIMER peripheral register block. [in] flagsPending LETIMER interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line
172
of file
em_letimer.h
.
Referenced by LETIMER_Reset() .
| __STATIC_INLINE void LETIMER_IntDisable | ( | LETIMER_TypeDef * |
letimer,
|
| uint32_t |
flags
|
||
| ) |
Disable one or more LETIMER interrupts.
- Parameters
-
[in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line
192
of file
em_letimer.h
.
| __STATIC_INLINE void LETIMER_IntEnable | ( | LETIMER_TypeDef * |
letimer,
|
| uint32_t |
flags
|
||
| ) |
Enable one or more LETIMER interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LETIMER_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] letimerPointer to the LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line
213
of file
em_letimer.h
.
| __STATIC_INLINE uint32_t LETIMER_IntGet | ( | LETIMER_TypeDef * |
letimer
|
) |
Get pending LETIMER interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
-
[in] letimerPointer to LETIMER peripheral register block.
- Returns
- LETIMER interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line
232
of file
em_letimer.h
.
| __STATIC_INLINE uint32_t LETIMER_IntGetEnabled | ( | LETIMER_TypeDef * |
letimer
|
) |
Get enabled and pending LETIMER interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
-
[in] letimerPointer to LETIMER peripheral register block.
- Returns
-
Pending and enabled LETIMER interrupt sources. Return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in LETIMER_IEN_nnn register (LETIMER_IEN_nnn) and
- the OR combination of valid interrupt flags of the LETIMER module (LETIMER_IF_nnn).
Definition at line
258
of file
em_letimer.h
.
| __STATIC_INLINE void LETIMER_IntSet | ( | LETIMER_TypeDef * |
letimer,
|
| uint32_t |
flags
|
||
| ) |
Set one or more pending LETIMER interrupts from SW.
- Parameters
-
[in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line
281
of file
em_letimer.h
.
| uint32_t LETIMER_RepeatGet | ( | LETIMER_TypeDef * |
letimer,
|
| unsigned int |
rep
|
||
| ) |
Get the LETIMER repeat register value.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat register to get, either 0 or 1.
- Returns
- Repeat register value, 0 if invalid register selected.
Definition at line
459
of file
em_letimer.c
.
| void LETIMER_RepeatSet | ( | LETIMER_TypeDef * |
letimer,
|
| unsigned int |
rep,
|
||
| uint32_t |
value
|
||
| ) |
Set the LETIMER repeat counter register value.
- Note
- The setting of a repeat counter register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat counter register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff).
Definition at line
511
of file
em_letimer.c
.
Referenced by MIC_init() .
| void LETIMER_Reset | ( | LETIMER_TypeDef * |
letimer
|
) |
Reset LETIMER to the same state that it was in after a hardware reset.
- Note
- The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block.
Definition at line
557
of file
em_letimer.c
.
References LETIMER_IntClear() , and LETIMER_SyncWait() .
| uint32_t LETIMER_TopGet | ( | LETIMER_TypeDef * |
letimer
|
) |
Get the current LETIMER top value.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block.
- Returns
- The top value. This will be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.
Definition at line
659
of file
em_letimer.c
.
| void LETIMER_TopSet | ( | LETIMER_TypeDef * |
letimer,
|
| uint32_t |
value
|
||
| ) |
Set the LETIMER top value.
- Note
- The LETIMER is a down-counter, so when the counter reaches 0 then the top value will be loaded into the counter. This function can be used to set the top value.
If the LETIMER is not already configured to use a top value then this function will enable that functionality for the user.
- Parameters
-
[in] letimerA pointer to the LETIMER peripheral register block. [in] valueThe top value. This can be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.
Definition at line
625
of file
em_letimer.c
.
References LETIMER_CompareSet() .