RAIL_AntennaConfig_t Struct Reference
A configuration for Antenna switch pins.
#include <
rail_chip_specific.h
>
Data Fields |
|
| bool | ant0PinEn |
|
MODEM_ROUTEPEN fields.
|
|
| bool | ant1PinEn |
|
Antenna 1 Pin Enable.
|
|
| uint8_t | ant0Loc |
|
MODEM_ROUTELOC1 fields.
|
|
| GPIO_Port_TypeDef | ant0Port |
|
Antenna 0 output GPIO port.
|
|
| uint8_t | ant0Pin |
|
Antenna 0 output GPIO pin.
|
|
| uint8_t | ant1Loc |
|
Antenna 1 location for pin/port.
|
|
| GPIO_Port_TypeDef | ant1Port |
|
Antenna 1 output GPIO port.
|
|
| uint8_t | ant1Pin |
|
Antenna 1 output GPIO pin.
|
|
A configuration for Antenna switch pins.
Definition at line
589
of file
rail_chip_specific.h
.
Field Documentation
| uint8_t RAIL_AntennaConfig_t::ant0Loc |
MODEM_ROUTELOC1 fields.
Antenna 0 location for pin/port
Definition at line
597
of file
rail_chip_specific.h
.
| bool RAIL_AntennaConfig_t::ant0PinEn |
MODEM_ROUTEPEN fields.
Antenna 0 Pin Enable
Definition at line
592
of file
rail_chip_specific.h
.
The documentation for this struct was generated from the following file:
-
chip/efr32/
rail_chip_specific.h