Detailed information requested and about the packet that was just transmitted.
#include <
rail_types.h
>
Data Fields | |
RAIL_PacketTimeStamp_t | timeSent |
The timestamp of the transmitted packet in the RAIL timebase, filled in by RAIL_GetTxPacketDetails(). | |
bool | isAck |
Indicates whether the transmitted packet was an ACK. |
Detailed information requested and about the packet that was just transmitted.
Definition at line 1471
of file rail_types.h
.
Field Documentation
bool RAIL_TxPacketDetails_t::isAck |
Indicates whether the transmitted packet was an ACK.
An 'ACK' is defined as a packet sent in response to a received ACK-requesting frame when auto ACK is enabled. Set to false for not an ACK and true for an ACK. It should always be set to false if auto ACK is not enabled.
Definition at line 1483
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h