RAIL_BLE_State_t Struct Reference
A state structure for BLE.
#include <
rail_ble.h
>
Data Fields |
|
| uint32_t | crcInit |
|
The value used to initialize the CRC algorithm.
|
|
| uint32_t | accessAddress |
|
The access address used for the connection.
|
|
| uint16_t | channel |
|
The logical channel used.
|
|
| bool | disableWhitening |
|
Indicates whether the whitening engine should be off.
|
|
A state structure for BLE.
This structure must be allocated in application global read-write memory that persists for the duration of BLE usage. It cannot be allocated in read-only memory or on the call stack.
Definition at line
96
of file
rail_ble.h
.
Field Documentation
| uint32_t RAIL_BLE_State_t::accessAddress |
The access address used for the connection.
Definition at line
98
of file
rail_ble.h
.
| uint16_t RAIL_BLE_State_t::channel |
The logical channel used.
Definition at line
99
of file
rail_ble.h
.
| uint32_t RAIL_BLE_State_t::crcInit |
The value used to initialize the CRC algorithm.
Definition at line
97
of file
rail_ble.h
.
| bool RAIL_BLE_State_t::disableWhitening |
Indicates whether the whitening engine should be off.
Definition at line
100
of file
rail_ble.h
.
The documentation for this struct was generated from the following file:
-
protocol/ble/
rail_ble.h