RAIL_PtiConfig_t Struct Reference
A configuration for PTI.
#include <
rail_chip_specific.h
>
Data Fields | |
RAIL_PtiMode_t | mode |
Packet Trace mode (UART or SPI) | |
uint32_t | baud |
Output baudrate for PTI in Hz. | |
uint8_t | doutLoc |
Data output (DOUT) location for pin/port. | |
GPIO_Port_TypeDef | doutPort |
Data output (DOUT) GPIO port. | |
uint8_t | doutPin |
Data output (DOUT) GPIO pin. | |
uint8_t | dclkLoc |
Data clock (DCLK) location for pin/port. | |
GPIO_Port_TypeDef | dclkPort |
Data clock (DCLK) GPIO port. | |
uint8_t | dclkPin |
Data clock (DCLK) GPIO pin. | |
uint8_t | dframeLoc |
Data frame (DFRAME) location for pin/port. | |
GPIO_Port_TypeDef | dframePort |
Data frame (DFRAME) GPIO port. | |
uint8_t | dframePin |
Data frame (DFRAME) GPIO pin. |
A configuration for PTI.
Definition at line 545
of file rail_chip_specific.h
.
Field Documentation
uint8_t RAIL_PtiConfig_t::dclkLoc |
Data clock (DCLK) location for pin/port.
Only used in SPI mode
Definition at line 557
of file rail_chip_specific.h
.
uint8_t RAIL_PtiConfig_t::dclkPin |
Data clock (DCLK) GPIO pin.
Only used in SPI mode
Definition at line 561
of file rail_chip_specific.h
.
GPIO_Port_TypeDef RAIL_PtiConfig_t::dclkPort |
Data clock (DCLK) GPIO port.
Only used in SPI mode
Definition at line 559
of file rail_chip_specific.h
.
uint8_t RAIL_PtiConfig_t::dframeLoc |
Data frame (DFRAME) location for pin/port.
Definition at line 563
of file rail_chip_specific.h
.
The documentation for this struct was generated from the following file:
- chip/efr32/
rail_chip_specific.h