RAIL_ChannelConfig_t Struct Reference
A channel configuration structure, which defines the channel meaning when a channel number is passed into a RAIL function, e.g., RAIL_StartTx() and RAIL_StartRx().
#include <
rail_types.h
>
Data Fields | |
const uint32_t * | phyConfigBase |
Base radio configuration for the corresponding channel configuration entries. | |
const uint32_t * | phyConfigDeltaSubtract |
Minimum radio configuration to restore channel entries back to base configuration. | |
const RAIL_ChannelConfigEntry_t * | configs |
Pointer to an array of RAIL_ChannelConfigEntry_t entries. | |
uint32_t | length |
Number of RAIL_ChannelConfigEntry_t entries. |
A channel configuration structure, which defines the channel meaning when a channel number is passed into a RAIL function, e.g., RAIL_StartTx() and RAIL_StartRx().
A RAIL_ChannelConfig_t structure defines the channel scheme that an application uses when registered in RAIL_ConfigChannels().
These are a few examples of different channel configurations:
Definition at line 1001
of file rail_types.h
.
Field Documentation
const RAIL_ChannelConfigEntry_t* RAIL_ChannelConfig_t::configs |
Pointer to an array of RAIL_ChannelConfigEntry_t entries.
Definition at line 1007
of file rail_types.h
.
uint32_t RAIL_ChannelConfig_t::length |
Number of RAIL_ChannelConfigEntry_t entries.
Definition at line 1010
of file rail_types.h
.
const uint32_t* RAIL_ChannelConfig_t::phyConfigBase |
Base radio configuration for the corresponding channel configuration entries.
Definition at line 1002
of file rail_types.h
.
const uint32_t* RAIL_ChannelConfig_t::phyConfigDeltaSubtract |
Minimum radio configuration to restore channel entries back to base configuration.
Definition at line 1004
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h