API messages in idle modeFULL_MAC_API > API messages by mode

WFM API messages applicable for an interface in idle mode.

Data Structures

struct sl_wfx_set_mac_address_req_t
Request message to set MAC address of the interface.
struct sl_wfx_set_mac_address_cnf_t
Confirmation message for sl_wfx_set_mac_address_req_t .
struct sl_wfx_connect_req_t
Request message for connecting to a Wi-Fi network.
struct sl_wfx_connect_cnf_t
Confirmation message for sl_wfx_connect_req_t .
struct sl_wfx_connect_ind_t
Indication message used to signal the completion of a connection operation.
struct sl_wfx_start_ap_req_t
Request message for starting a Wi-Fi network.
struct sl_wfx_start_ap_cnf_t
Confirmation message for sl_wfx_start_ap_req_t .
struct sl_wfx_start_ap_ind_t
Indication message used to signal the completion of a start request.
struct sl_wfx_start_scan_req_t
Request message for starting a scan to detect near-by access points.
struct sl_wfx_start_scan_cnf_t
Confirmation message for sl_wfx_start_scan_req_t .
struct sl_wfx_stop_scan_cnf_t
Confirmation message for sl_wfx_stop_scan_req_t .
struct sl_wfx_scan_result_ind_t
Indication message used to signal an access point has been detected.
struct sl_wfx_scan_complete_ind_t
Indication message used to signal a scan was completed.
struct sl_wfx_join_ibss_req_t
Request message for connecting to or starting an IBSS network.
struct sl_wfx_join_ibss_cnf_t
Confirmation message for sl_wfx_join_ibss_req_t .
struct sl_wfx_join_ibss_ind_t
Indication message used to signal the completion of a join request.
struct sl_wfx_set_roam_parameters_req_t
Request message for setting the roaming parameters.
struct sl_wfx_set_roam_parameters_cnf_t
Confirmation message for sl_wfx_set_roam_parameters_req_t .
struct sl_wfx_set_tx_rate_parameters_req_t
Request message for setting the TX rate set parameters.
struct sl_wfx_set_tx_rate_parameters_cnf_t
Confirmation message for sl_wfx_set_tx_rate_parameters_req_t .
struct sl_wfx_set_scan_parameters_req_t
Request message for setting scan parameters.
struct sl_wfx_set_max_tx_power_req_t
Request message for setting the maximum transmit power of the device.
struct sl_wfx_set_max_tx_power_cnf_t
Confirmation message for sl_wfx_set_max_tx_power_req_t .
struct sl_wfx_get_max_tx_power_cnf_t
Confirmation message for sl_wfx_get_max_tx_power_req_t .
struct sl_wfx_stop_scan_req_t
Request message for stopping an ongoing scan.
struct sl_wfx_get_max_tx_power_req_t
Request message for getting the maximum transmit power.

Detailed Description

WFM API messages applicable for an interface in idle mode.


Data Structure Documentation

◆ sl_wfx_set_mac_address_req_t

struct sl_wfx_set_mac_address_req_t

Request message to set MAC address of the interface.

The host can use this request to set the MAC address of an interface. If not set, the device will use a built-in MAC address. Note that if multiple interfaces are used, the MAC address MUST be different on each interface.

Interface mode Request allowed
idle Yes
station No
AP No
IBSS No


Definition at line 734 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_mac_address_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_mac_address_cnf_t

struct sl_wfx_set_mac_address_cnf_t

Confirmation message for sl_wfx_set_mac_address_req_t .

Definition at line 758 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_mac_address_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_connect_req_t

struct sl_wfx_connect_req_t

Request message for connecting to a Wi-Fi network.

The host can use this request to initiate a connection to a Wi-Fi network. An ongoing connection attempt can be canceled by sending sl_wfx_disconnect_req_t message. Completion of the connection request will be signaled by sl_wfx_connect_ind_t message. It may take up to 10 seconds to receive the message.

Interface mode Request allowed
idle Yes
station No
AP No
IBSS No


Definition at line 852 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_connect_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_connect_cnf_t

struct sl_wfx_connect_cnf_t

Confirmation message for sl_wfx_connect_req_t .

Definition at line 876 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_connect_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_connect_ind_t

struct sl_wfx_connect_ind_t

Indication message used to signal the completion of a connection operation.

The device will send this indication to signal the connection request initiated with sl_wfx_connect_req_t has been completed. The indication is also sent when the device autonomously roams to another access point.

Definition at line 926 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_connect_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_start_ap_req_t

struct sl_wfx_start_ap_req_t

Request message for starting a Wi-Fi network.

The host can use this request to initiate a Wi-Fi network.

Interface mode Request allowed
idle Yes
station No
AP No
IBSS No


Definition at line 1208 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_start_ap_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_start_ap_cnf_t

struct sl_wfx_start_ap_cnf_t

Confirmation message for sl_wfx_start_ap_req_t .

Definition at line 1232 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_start_ap_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_start_ap_ind_t

struct sl_wfx_start_ap_ind_t

Indication message used to signal the completion of a start request.

The device will send this indication to signal the start request initiated with sl_wfx_start_ap_req_t has been completed.

Definition at line 1258 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_start_ap_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_start_scan_req_t

struct sl_wfx_start_scan_req_t

Request message for starting a scan to detect near-by access points.

The host can use this request to start a scan operation to detect near-by access points.

Interface mode Request allowed
idle Yes
station Yes
AP No
IBSS No


Definition at line 1716 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_start_scan_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_start_scan_cnf_t

struct sl_wfx_start_scan_cnf_t

Confirmation message for sl_wfx_start_scan_req_t .

Definition at line 1741 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_start_scan_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_stop_scan_cnf_t

struct sl_wfx_stop_scan_cnf_t

Confirmation message for sl_wfx_stop_scan_req_t .

Definition at line 1781 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_stop_scan_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_scan_result_ind_t

struct sl_wfx_scan_result_ind_t

Indication message used to signal an access point has been detected.

The device will send this indication to signal an access point has has been detected during the scan operation.

Definition at line 1839 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_scan_result_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_scan_complete_ind_t

struct sl_wfx_scan_complete_ind_t

Indication message used to signal a scan was completed.

The device will send this indication to signal a scan operation has been completed.

Definition at line 1866 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_scan_complete_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_join_ibss_req_t

struct sl_wfx_join_ibss_req_t

Request message for connecting to or starting an IBSS network.

The host can use this request to connect to an IBSS network. If no existing network is found, the device will start a new network.

Interface mode Request allowed
idle Yes
station No
AP No
IBSS No


Definition at line 1921 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_join_ibss_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_join_ibss_cnf_t

struct sl_wfx_join_ibss_cnf_t

Confirmation message for sl_wfx_join_ibss_req_t .

Definition at line 1945 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_join_ibss_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_join_ibss_ind_t

struct sl_wfx_join_ibss_ind_t

Indication message used to signal the completion of a join request.

The device will send this indication to signal the join request initiated with sl_wfx_join_ibss_req_t has been completed.

Definition at line 1980 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_join_ibss_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_roam_parameters_req_t

struct sl_wfx_set_roam_parameters_req_t

Request message for setting the roaming parameters.

The host can use this request to configure the roaming parameters used by the device.
See Roaming for further details.

Interface mode Request allowed
idle Yes
station Yes
AP No
IBSS No


Definition at line 2346 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_roam_parameters_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_roam_parameters_cnf_t

struct sl_wfx_set_roam_parameters_cnf_t

Confirmation message for sl_wfx_set_roam_parameters_req_t .

Definition at line 2371 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_roam_parameters_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_tx_rate_parameters_req_t

struct sl_wfx_set_tx_rate_parameters_req_t

Request message for setting the TX rate set parameters.

The host can use this request to configure the TX rate set parameters of the device. The rate set determines what data rates will be used by the device to transmit data frames.

Interface mode Request allowed
idle Yes
station Yes
AP No
IBSS No


Definition at line 2413 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_tx_rate_parameters_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_tx_rate_parameters_cnf_t

struct sl_wfx_set_tx_rate_parameters_cnf_t

Confirmation message for sl_wfx_set_tx_rate_parameters_req_t .

Definition at line 2438 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_tx_rate_parameters_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_scan_parameters_req_t

struct sl_wfx_set_scan_parameters_req_t

Request message for setting scan parameters.

The host can use this request to configure the scan parameters used by the device.

Interface mode Request allowed
idle Yes
station Yes
AP No
IBSS No


Definition at line 2676 of file sl_wfx_cmd_api.h .

◆ sl_wfx_set_max_tx_power_req_t

struct sl_wfx_set_max_tx_power_req_t

Request message for setting the maximum transmit power of the device.

The host can use this request to set a maximum transmit power. The device can still use a lower transmit power depending on regulatory rules or internal limitations.

Interface mode Request allowed
idle Yes
station Yes
AP Yes
IBSS Yes


Definition at line 2923 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_max_tx_power_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_tx_power_cnf_t

struct sl_wfx_set_max_tx_power_cnf_t

Confirmation message for sl_wfx_set_max_tx_power_req_t .

Definition at line 2950 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_set_max_tx_power_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_get_max_tx_power_cnf_t

struct sl_wfx_get_max_tx_power_cnf_t

Confirmation message for sl_wfx_get_max_tx_power_req_t .

Definition at line 3004 of file sl_wfx_cmd_api.h .

Data Fields
sl_wfx_get_max_tx_power_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_stop_scan_req_t

struct sl_wfx_stop_scan_req_t

Request message for stopping an ongoing scan.

The host can use this request to stop an ongoing scan operation.

Interface mode Request allowed
idle Yes
station Yes
AP No
IBSS No

◆ sl_wfx_get_max_tx_power_req_t

struct sl_wfx_get_max_tx_power_req_t

Request message for getting the maximum transmit power.

The host can use this request to get the current value of maximum transmit power.

Interface mode Request allowed
idle Yes
station Yes
AP Yes
IBSS Yes