Structure representing the BLE accept list.

This structure is used to define the parameters for the BLE accept list, which includes the operation to add or delete the address, the device address, and the address type.

Public Attributes#

uint8_t

Public Attribute Documentation#

addordeltowhitlist#

uint8_t rsi_ble_accept_list_s::addordeltowhitlist

Bit used to add or delete the address from/to the allow list


dev_addr#

uint8_t rsi_ble_accept_list_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the device


bdaddressType#

uint8_t rsi_ble_accept_list_s::bdaddressType

Address type