Structure represents the BLE Advertising Extensions (AE) command to read the supported maximum advertising data.

This structure is used to define the parameters for a BLE AE command to read the supported maximum advertising data, which includes a reserved field for future use or alignment.

Public Attributes#

uint16_t

Public Attribute Documentation#

reserved#

uint16_t rsi_ble_ae_read_supported_max_adv_data_s::reserved

Reserved field for future use or alignment