Structure representing the BLE connection request.

This structure is used to define the parameters for a BLE connection request, which includes the address type and address of the device to connect, scan interval, scan window, connection interval, connection latency, and supervision timeout.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

dev_addr_type#

uint8_t rsi_ble_req_conn_s::dev_addr_type

Address type of the device to connect


dev_addr#

uint8_t rsi_ble_req_conn_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the device to connect


le_scan_interval#

uint16_t rsi_ble_req_conn_s::le_scan_interval

Scan interval


le_scan_window#

uint16_t rsi_ble_req_conn_s::le_scan_window

Scan window


conn_interval_min#

uint16_t rsi_ble_req_conn_s::conn_interval_min

Minimum connection interval


conn_interval_max#

uint16_t rsi_ble_req_conn_s::conn_interval_max

Maximum connection interval


conn_latency#

uint16_t rsi_ble_req_conn_s::conn_latency

Connection latency


supervision_tout#

uint16_t rsi_ble_req_conn_s::supervision_tout

Supervision timeout