Structure represents the BLE Security Manager Protocol (SMP) pairing request.

This structure is used to define the parameters for a BLE SMP pairing request, which includes the device address, IO capability, and MITM (Man-In-The-Middle) protection requirement.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_smp_pair_s::dev_addr[RSI_DEV_ADDR_LEN]

Device address for the pairing request


io_capability#

uint8_t rsi_ble_req_smp_pair_s::io_capability

IO capability of the device


mitm_req#

uint8_t rsi_ble_req_smp_pair_s::mitm_req

MITM (Man-In-The-Middle) protection requirement