Structure represents the BLE command to set an attribute value.

This structure is used to define the parameters for a BLE command to set an attribute value, which includes the remote device address, the attribute handle, the length of the attribute value, and the attribute value itself. The module won't receive the acknowledgement from the remote device.

Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_set_att_cmd_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


handle#

uint8_t rsi_ble_set_att_cmd_s::handle[2]

Attribute handle


length#

uint8_t rsi_ble_set_att_cmd_s::length

Length of the attribute value


att_value#

uint8_t rsi_ble_set_att_cmd_s::att_value[RSI_DEV_ATT_LEN]

Attribute value