Structure represents the BLE Security Manager Protocol (SMP) pairing failure request.

This structure is used to define the parameters for a BLE SMP pairing failure request, which includes the address of the remote device and the reason for the pairing failure.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_smp_pair_failed_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the remote device


reason#

uint8_t rsi_ble_req_smp_pair_failed_s::reason

Reason for the pairing failure