Structure represents the BLE end test mode parameters.

This structure is used to define the parameter for a BLE end test mode. Number of TX / RX packets received are displayed when test is stopped.

Public Attributes#

uint16_t

Public Attribute Documentation#

num_of_pkts#

uint16_t rsi_ble_end_test_mode_s::num_of_pkts

Number of TX / RX packets received when test is stopped