Structure represents the BLE command to get the LE ping timeout.

This structure is used to define the parameters for a BLE command to get the LE ping timeout, which includes the remote device address.

Public Attributes#

uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_get_le_ping_timeout_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address (6 bytes)