Structure represents the BLE operation mode.

This structure is used to define the parameters for the BLE operation mode, that includes Bluetooth features, and the module type.

Public Attributes#

uint32_t

Public Attribute Documentation#

bt_features#

uint32_t rsi_ble_oper_mode_s::bt_features

Bluetooth features


module_type#

uint8_t rsi_ble_oper_mode_s::module_type

Module type