BR parameter set.
Public Attributes#
PAN configuration parameter set.
DHCP server parameter set.
PAN discovery parameter set.
Authentication parameter set.
uint8_t
Enable FAN 1.0 router node support PAN-wide.
LFN parent parameter set.
Misc parameter set.
MPL parameter set.
uint32_t
Maximum number of nodes supported by border router at once.
RPL parameter set.
uint32_t
Version of this API.
Public Attribute Documentation#
configuration#
sl_wisun_br_params_configuration sl_wisun_br_connection_params_t::configuration
PAN configuration parameter set.
discovery#
sl_wisun_br_params_discovery sl_wisun_br_connection_params_t::discovery
PAN discovery parameter set.
enable_ffn10#
uint8_t sl_wisun_br_connection_params_t::enable_ffn10
Enable FAN 1.0 router node support PAN-wide.
lfn_parent#
sl_wisun_br_params_lfn_parent sl_wisun_br_connection_params_t::lfn_parent
LFN parent parameter set.
pan_capacity#
uint32_t sl_wisun_br_connection_params_t::pan_capacity
Maximum number of nodes supported by border router at once.
version#
uint32_t sl_wisun_br_connection_params_t::version
Version of this API.
This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.