Channel mask.

Public Attributes#

uint8_t

Bit mask of channels.

Public Attribute Documentation#

mask#

uint8_t sl_wisun_channel_mask_t::mask[SL_WISUN_CHANNEL_MASK_SIZE]

Bit mask of channels.

This field specifies a bit mask of channels, one bit per channel. First byte of the array represents channel numbers 0 - 7, with bit 0 being channel 0. Second byte represents channel numbers 8 - 15 and so forth.


Definition at line 656 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h