LFN data layer parameters.
Public Attributes#
The LFN assumes its parent is lost after [lfn_maintain_parent_time] number of Broadcast sync periods with no message received from its parent.
Reserved, set to zero.
Maximum acceptable LFN unicast interval (milliseconds)
Minimum acceptable LFN unicast interval (milliseconds)
Initial LFN Unicast interval proposed by the LFN (milliseconds).
Public Attribute Documentation#
lfn_maintain_parent_time#
uint8_t sl_wisun_lfn_params_data_layer_t::lfn_maintain_parent_time
The LFN assumes its parent is lost after [lfn_maintain_parent_time] number of Broadcast sync periods with no message received from its parent.
Specification range [1, 60]
75
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
reserved#
uint8_t sl_wisun_lfn_params_data_layer_t::reserved[3]
Reserved, set to zero.
77
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
unicast_interval_max_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_max_ms
Maximum acceptable LFN unicast interval (milliseconds)
71
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
unicast_interval_min_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_min_ms
Minimum acceptable LFN unicast interval (milliseconds)
69
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
unicast_interval_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_ms
Initial LFN Unicast interval proposed by the LFN (milliseconds).
The real unicast interval duration is negotiated with the LFN parent, between unicast_interval_min_ms and unicast_interval_max_ms.
67
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h