Adaptive rate algorithm rate stats.

Public Attributes#

uint16_t

Number of tx without acknowledgement.

uint32_t

Frame tx time.

int8_t

Indicates if the rate can be probed.

uint8_t

Reserved, set to zero.

uint32_t

Number of times the rate was selected.

uint8_t

Number of times this rate was skipped.

uint16_t

Number of successful transmissions.

float

Estimated chance of success.

float

Estimated troughput in kb/s.

Public Attribute Documentation#

fail_count#

uint16_t sl_wisun_rate_stats_t::fail_count

Number of tx without acknowledgement.


Definition at line 849 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

frame_duration_us#

uint32_t sl_wisun_rate_stats_t::frame_duration_us

Frame tx time.


Definition at line 839 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

probe_limit#

int8_t sl_wisun_rate_stats_t::probe_limit

Indicates if the rate can be probed.


Definition at line 853 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

reserved#

uint8_t sl_wisun_rate_stats_t::reserved[2]

Reserved, set to zero.


Definition at line 855 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

sample_count#

uint32_t sl_wisun_rate_stats_t::sample_count

Number of times the rate was selected.


Definition at line 841 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

skipped_sample_count#

uint8_t sl_wisun_rate_stats_t::skipped_sample_count

Number of times this rate was skipped.


Definition at line 851 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

success_count#

uint16_t sl_wisun_rate_stats_t::success_count

Number of successful transmissions.


Definition at line 847 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

success_probability#

float sl_wisun_rate_stats_t::success_probability

Estimated chance of success.


Definition at line 843 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

throughput#

float sl_wisun_rate_stats_t::throughput

Estimated troughput in kb/s.


Definition at line 845 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h