MPL parameter set.

Public Attributes#

uint8_t

MPL seed-id type, 0 indicates the seed-id is elided and is the IPv6 source address, 3 indicates the seed-id is the 128-bit ULA/GUA of the source.

uint16_t

MPL seed set entry lifetime (seconds)

uint8_t

MPL trickle timer expirations.

Public Attribute Documentation#

seed_id_type#

uint8_t sl_wisun_params_mpl::seed_id_type

MPL seed-id type, 0 indicates the seed-id is elided and is the IPv6 source address, 3 indicates the seed-id is the 128-bit ULA/GUA of the source.


Definition at line 219 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

seed_set_entry_lifetime_s#

uint16_t sl_wisun_params_mpl::seed_set_entry_lifetime_s

MPL seed set entry lifetime (seconds)


Definition at line 213 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

trickle#

sl_wisun_trickle_params_t sl_wisun_params_mpl::trickle

MPL trickle timer.


Definition at line 211 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

trickle_expirations#

uint8_t sl_wisun_params_mpl::trickle_expirations

MPL trickle timer expirations.


Definition at line 215 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h