Predefined BR parameter sets#

Predefined BR parameter sets for sl_wisun_br_set_connection_parameters().

These parameter sets can be used either as-is to replicate the behavior of sl_wisun_br_set_network_size(), or used as an initialization value for an application-specific parameter set.

Variables#

Profile for development (shorter connection time)

Variable Documentation#

SL_WISUN_BR_PARAMS_PROFILE_LARGE#

const sl_wisun_br_connection_params_t SL_WISUN_BR_PARAMS_PROFILE_LARGE

Profile for a large network.


Definition at line 406 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h

SL_WISUN_BR_PARAMS_PROFILE_MEDIUM#

const sl_wisun_br_connection_params_t SL_WISUN_BR_PARAMS_PROFILE_MEDIUM

Profile for a medium network.


Definition at line 335 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h

SL_WISUN_BR_PARAMS_PROFILE_SMALL#

const sl_wisun_br_connection_params_t SL_WISUN_BR_PARAMS_PROFILE_SMALL

Profile for a small network.


Definition at line 264 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h

SL_WISUN_BR_PARAMS_PROFILE_TEST#

const sl_wisun_br_connection_params_t SL_WISUN_BR_PARAMS_PROFILE_TEST

Profile for development (shorter connection time)


Definition at line 193 of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h