Authentication parameter set.
Public Attributes#
If true, allow join state 2 to be skipped using cached credentials from the previous connection.
GTK_MAX_MISMATCH (minutes)
GTK_REQUEST_IMAX (minutes)
GTK_REQUEST_IMIN (minutes)
Initial EAPOL-Key first Tx max delay (seconds)
Initial EAPOL-Key first Tx min delay (seconds)
Initial EAPOL-Key retry limit.
Initial EAPOL-Key retry exponential backoff max limit (seconds)
Initial EAPOL-Key retry exponential backoff max (seconds)
Initial EAPOL-Key retry exponential backoff min (seconds)
LGTK_MAX_MISMATCH (minutes)
PMK lifetime (minutes)
PTK lifetime (minutes)
Reserved, set to zero.
Security protocol retry timeout (seconds)
Security protocol trickle timer.
Security protocol trickle timer expirations.
Temporary neighbor link minimum timeout (seconds)
Public Attribute Documentation#
allow_skip#
uint8_t sl_wisun_params_eapol::allow_skip
If true, allow join state 2 to be skipped using cached credentials from the previous connection.
167
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
gtk_max_mismatch_m#
uint16_t sl_wisun_params_eapol::gtk_max_mismatch_m
GTK_MAX_MISMATCH (minutes)
158
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
gtk_request_imax_m#
uint16_t sl_wisun_params_eapol::gtk_request_imax_m
GTK_REQUEST_IMAX (minutes)
156
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
gtk_request_imin_m#
uint16_t sl_wisun_params_eapol::gtk_request_imin_m
GTK_REQUEST_IMIN (minutes)
154
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
initial_key_max_s#
uint16_t sl_wisun_params_eapol::initial_key_max_s
Initial EAPOL-Key first Tx max delay (seconds)
144
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
initial_key_min_s#
uint16_t sl_wisun_params_eapol::initial_key_min_s
Initial EAPOL-Key first Tx min delay (seconds)
142
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
initial_key_retry_limit#
uint8_t sl_wisun_params_eapol::initial_key_retry_limit
Initial EAPOL-Key retry limit.
164
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
initial_key_retry_max_limit_s#
uint16_t sl_wisun_params_eapol::initial_key_retry_max_limit_s
Initial EAPOL-Key retry exponential backoff max limit (seconds)
150
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
initial_key_retry_max_s#
uint16_t sl_wisun_params_eapol::initial_key_retry_max_s
Initial EAPOL-Key retry exponential backoff max (seconds)
148
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
initial_key_retry_min_s#
uint16_t sl_wisun_params_eapol::initial_key_retry_min_s
Initial EAPOL-Key retry exponential backoff min (seconds)
146
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
lgtk_max_mismatch_m#
uint16_t sl_wisun_params_eapol::lgtk_max_mismatch_m
LGTK_MAX_MISMATCH (minutes)
160
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
pmk_lifetime_m#
uint32_t sl_wisun_params_eapol::pmk_lifetime_m
PMK lifetime (minutes)
136
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
ptk_lifetime_m#
uint32_t sl_wisun_params_eapol::ptk_lifetime_m
PTK lifetime (minutes)
138
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
reserved#
uint8_t sl_wisun_params_eapol::reserved[3]
Reserved, set to zero.
169
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
sec_prot_retry_timeout_s#
uint16_t sl_wisun_params_eapol::sec_prot_retry_timeout_s
Security protocol retry timeout (seconds)
140
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
sec_prot_trickle#
sl_wisun_trickle_params_t sl_wisun_params_eapol::sec_prot_trickle
Security protocol trickle timer.
134
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
sec_prot_trickle_expirations#
uint8_t sl_wisun_params_eapol::sec_prot_trickle_expirations
Security protocol trickle timer expirations.
162
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
temp_min_timeout_s#
uint16_t sl_wisun_params_eapol::temp_min_timeout_s
Temporary neighbor link minimum timeout (seconds)
152
of file /mnt/raid/workspaces/ws.obQFDUprC/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h