Public Attributes#
void(*
uint8_t
Will be returned with transmit status Allows application to recognize frames.
uint8_t
Number of new destinations Array containing new destinations.
Public Attribute Documentation#
Handle#
void(* SRequestNewRouteDestinations::Handle) (void)
Definition at line
1758
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
iDestinationCount#
uint8_t SRequestNewRouteDestinations::iDestinationCount
Will be returned with transmit status Allows application to recognize frames.
Definition at line
1760
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
aNewDestinations#
uint8_t SRequestNewRouteDestinations::aNewDestinations[ZW_MAX_CACHED_RETURN_ROUTE_DESTINATIONS]
Number of new destinations Array containing new destinations.
Definition at line
1762
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h