Transmit Parameters Union used by SZwaveTransmitPackage.

Public Attribute Documentation#

ExploreInclusionRequest#

SExploreInclusionRequest UTransmitParameters::ExploreInclusionRequest

Definition at line 2008 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

ExploreExclusionRequest#

SExploreExclusionRequest UTransmitParameters::ExploreExclusionRequest

Definition at line 2009 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

NetworkUpdateRequest#

SNetworkUpdateRequest UTransmitParameters::NetworkUpdateRequest

Definition at line 2010 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

NodeInfoRequest#

SNodeInfoRequest UTransmitParameters::NodeInfoRequest

Definition at line 2011 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

NodeInfo#

SNodeInfo UTransmitParameters::NodeInfo

Definition at line 2012 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

IncludedNodeInfo#

SIncludedNodeInfo UTransmitParameters::IncludedNodeInfo

Definition at line 2013 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

Test#

STest UTransmitParameters::Test

Definition at line 2014 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendData#

SSendData UTransmitParameters::SendData

Definition at line 2016 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendDataEx#

SSendDataEx UTransmitParameters::SendDataEx

Definition at line 2017 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendDataBridge#

SSendDataBridge UTransmitParameters::SendDataBridge

Definition at line 2018 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendDataMulti#

SSendDataMulti UTransmitParameters::SendDataMulti

Definition at line 2019 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendDataMultiEx#

SSendDataMultiEx UTransmitParameters::SendDataMultiEx

Definition at line 2020 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendDataMultiBridge#

SSendDataMultiBridge UTransmitParameters::SendDataMultiBridge

Definition at line 2021 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SetSucNodeId#

SSetSucNodeId UTransmitParameters::SetSucNodeId

Definition at line 2023 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendSucNodeId#

SSendSucNodeId UTransmitParameters::SendSucNodeId

Definition at line 2024 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

AssignReturnRoute#

SAssignReturnRoute UTransmitParameters::AssignReturnRoute

Definition at line 2025 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

DeleteReturnRoute#

SDeleteReturnRoute UTransmitParameters::DeleteReturnRoute

Definition at line 2026 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendReplication#

SSendReplication UTransmitParameters::SendReplication

Definition at line 2027 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendReplicationReceiveComplete#

SSendReplicationReceiveComplete UTransmitParameters::SendReplicationReceiveComplete

Definition at line 2028 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SendSlaveNodeInformation#

SSendSlaveNodeInformation UTransmitParameters::SendSlaveNodeInformation

Definition at line 2029 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

RequestNewRouteDestinations#

SRequestNewRouteDestinations UTransmitParameters::RequestNewRouteDestinations

Definition at line 2031 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h