Public Attributes#

void(*

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.

Public Attribute Documentation#

Handle#

void(* SSendSucNodeId::Handle) (void)

Definition at line 1381 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

DestNodeId#

node_id_t SSendSucNodeId::DestNodeId

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.


Definition at line 1384 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

TransmitOptions#

uint8_t SSendSucNodeId::TransmitOptions

Definition at line 1385 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h