Public Attribute Documentation#

allocateMemoryForResponses#

bool EmberAfGbzMessageCreatorState::allocateMemoryForResponses

Definition at line 175 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

command#

uint8_t* EmberAfGbzMessageCreatorState::command

Definition at line 178 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

commandIndex#

uint16_t EmberAfGbzMessageCreatorState::commandIndex

Definition at line 179 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

commandLength#

uint16_t EmberAfGbzMessageCreatorState::commandLength

Definition at line 180 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

responses#

EmAfGbzUseCaseSpecificComponent* EmberAfGbzMessageCreatorState::responses

Definition at line 183 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

lastResponse#

EmAfGbzUseCaseSpecificComponent* EmberAfGbzMessageCreatorState::lastResponse

Definition at line 184 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

header#

EmAfGbzPayloadHeader* EmberAfGbzMessageCreatorState::header

Definition at line 185 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

nextEncryptedComponentZclSequenceNumber#

uint8_t EmberAfGbzMessageCreatorState::nextEncryptedComponentZclSequenceNumber

Definition at line 188 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

nextComponentZclSequenceNumber#

uint8_t EmberAfGbzMessageCreatorState::nextComponentZclSequenceNumber

Definition at line 189 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

nextAdditionalHeaderFrameCounter#

uint8_t EmberAfGbzMessageCreatorState::nextAdditionalHeaderFrameCounter

Definition at line 190 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

componentsCount#

uint8_t* EmberAfGbzMessageCreatorState::componentsCount

Definition at line 191 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

lastExtHeaderControlField#

uint8_t* EmberAfGbzMessageCreatorState::lastExtHeaderControlField

Definition at line 192 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

messageCode#

uint16_t EmberAfGbzMessageCreatorState::messageCode

Definition at line 193 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h

result#

EmberAfGbzMessageCreatorResult EmberAfGbzMessageCreatorState::result

Definition at line 196 of file app/framework/plugin/gbz-message-controller/gbz-message-controller.h