Structure for ZCL command "QueryNextImageRequest" from "Over the Air Bootloading".
Public Attribute Documentation#
fieldControl#
uint8_t __zcl_over_the_air_bootloading_cluster_query_next_image_request_command::fieldControl
manufacturerId#
uint16_t __zcl_over_the_air_bootloading_cluster_query_next_image_request_command::manufacturerId
imageType#
uint16_t __zcl_over_the_air_bootloading_cluster_query_next_image_request_command::imageType
currentFileVersion#
uint32_t __zcl_over_the_air_bootloading_cluster_query_next_image_request_command::currentFileVersion
hardwareVersion#
uint16_t __zcl_over_the_air_bootloading_cluster_query_next_image_request_command::hardwareVersion