Structure for ZCL command "QuerySpecificFileResponse" from "Over the Air Bootloading".
Public Attribute Documentation#
manufacturerId#
uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_response_command::manufacturerId
imageType#
uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_response_command::imageType
fileVersion#
uint32_t __zcl_over_the_air_bootloading_cluster_query_specific_file_response_command::fileVersion
imageSize#
uint32_t __zcl_over_the_air_bootloading_cluster_query_specific_file_response_command::imageSize