Green Power Server#

Callbacks for Green Power Server Component.

Callbacks#

void
sl_zigbee_af_green_power_server_commissioning_timeout_cb(uint8_t commissioningTimeoutType, uint8_t numberOfEndpoints, uint8_t *endpoint)

Green Power Server commissioning timeout callback.

void
sl_zigbee_af_green_power_server_pairing_complete_cb(uint8_t numberOfEndpoints, uint8_t *endpoint)

Green Power Server pairing complete callback.

bool
sl_zigbee_af_green_power_server_sink_table_access_notification_cb(void *data, sl_zigbee_af_gp_server_sink_table_access_type_t accessType)

Sink table access notification callback.

bool
sl_zigbee_af_green_power_server_gpd_commissioning_cb(sl_zigbee_gp_application_info_t *appInfo, bool *matchFound)

Green Power Server commissioning callback.

void

Green Power Server security failure callback.

bool

Green Power Server update involved TC callback.

bool
sl_zigbee_af_green_power_cluster_gp_notification_forward_cb(uint16_t options, sl_zigbee_gp_address_t *addr, uint32_t gpdSecurityFrameCounter, uint8_t gpdCommandId, uint8_t *gpdCommandPayload, uint16_t gppShortAddress, uint8_t gppDistance)

Green Power Server notification forward callback.

bool
sl_zigbee_af_green_power_server_gpd_commissioning_notification_cb(uint8_t commandId, uint16_t commNotificationOptions, sl_zigbee_gp_address_t *gpdAddr, uint32_t gpdSecurityFrameCounter, uint8_t gpdCommandId, uint8_t *gpdCommandPayload, uint16_t gppShortAddress, int8_t rssi, uint8_t linkQuality, uint8_t gppDistance, uint32_t commissioningNotificationMic)

Green Power Commissioning notification callback.

void
sl_zigbee_af_green_power_cluster_commissioning_message_status_notification_cb(sl_zigbee_af_green_power_server_commissioning_state_t *commissioningState, sl_zigbee_aps_frame_t *apsFrame, sl_zigbee_outgoing_message_type_t messageType, uint16_t destination, sl_status_t status)

Sink commissioning enter call status notification callback.

bool
sl_zigbee_af_green_power_server_update_alias_cb(sl_zigbee_gp_address_t *gpdAddr, uint16_t *alias)

Update alias information callback.

void
sl_zigbee_af_green_power_server_pairing_status_cb(sl_zigbee_sink_pairing_status_t status, sl_zigbee_commissioning_gpd_t *commissioningGpd)

Green Power Server pairing complete callback.

void
sl_zigbee_af_green_power_server_pre_sink_pairing_cb(sl_zigbee_commissioning_gpd_t *commissioningGpd)

Green power server update sink list callback.

Callbacks Documentation#

sl_zigbee_af_green_power_server_commissioning_timeout_cb#

void sl_zigbee_af_green_power_server_commissioning_timeout_cb (uint8_t commissioningTimeoutType, uint8_t numberOfEndpoints, uint8_t * endpoint)

Green Power Server commissioning timeout callback.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]commissioningTimeoutType

one of the types COMMISSIONING_TIMEOUT_TYPE_COMMISSIONING_WINDOW_TIMEOUT, COMMISSIONING_TIMEOUT_TYPE_GENERIC_SWITCH or COMMISSIONING_TIMEOUT_TYPE_MULTI_SENSOR

uint8_t[in]numberOfEndpoints

Number of sink endpoints participated in the commissioning

uint8_t *[in]endpoint

List of sink endpoints

This function is called by the Green Power Server upon expiration of any of the commissioning timers, which can be server commissioning window, generic switch commissioning, or multi-sensor commissioning timer expiration.


sl_zigbee_af_green_power_server_pairing_complete_cb#

void sl_zigbee_af_green_power_server_pairing_complete_cb (uint8_t numberOfEndpoints, uint8_t * endpoint)

Green Power Server pairing complete callback.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]numberOfEndpoints

Number of sink endpoints participated in the pairing

uint8_t *[in]endpoint

List of sink endpoints

This function is called by the Green Power Server upon the completion of the pairing to indicate the closure of the pairing session.


sl_zigbee_af_green_power_server_sink_table_access_notification_cb#

bool sl_zigbee_af_green_power_server_sink_table_access_notification_cb (void * data, sl_zigbee_af_gp_server_sink_table_access_type_t accessType)

Sink table access notification callback.

Parameters
TypeDirectionArgument NameDescription
void *[in]data

Pointer to data

sl_zigbee_af_gp_server_sink_table_access_type_t[in]accessType

Access type

This function is called by the Green Power Server plugin to notify the application about Green Power Device addition or removal by the green power server to the Sink Table. If returned false, the sink table remains un-accessed.

Returns

  • true if the access is granted.


sl_zigbee_af_green_power_server_gpd_commissioning_cb#

bool sl_zigbee_af_green_power_server_gpd_commissioning_cb (sl_zigbee_gp_application_info_t * appInfo, bool * matchFound)

Green Power Server commissioning callback.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_gp_application_info_t *[in]appInfo

Application information of the commissioning GPD.

bool *[out]matchFound

Output flag to notify matching functionality.

This function is called by the Green Power Server plugin to notify the application of a Green Power Device that has requested commissioning with this sink. Returns false if callback is not handled, true if callback is handled. When the callback is handled, it must set the matchFound argument appropriately to indicate if the matching functionality is found on the sink or not.

Returns

  • True if application handled it


sl_zigbee_af_green_power_server_gpd_security_failure_cb#

void sl_zigbee_af_green_power_server_gpd_security_failure_cb (sl_zigbee_gp_address_t * gpdAddr)

Green Power Server security failure callback.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_gp_address_t *[in]gpdAddr

This function is called by the Green Power Server plugin to notify the application of a Green Power Security Processing failed for an incoming notification.


sl_zigbee_af_green_power_server_update_involve_t_c_cb#

bool sl_zigbee_af_green_power_server_update_involve_t_c_cb (sl_status_t status)

Green Power Server update involved TC callback.

Parameters
TypeDirectionArgument NameDescription
sl_status_t[in]status

This function is called by the Green Power Server to proceed with updating the InvolveTC bit of the security level attribute.

Returns

  • True if application handled it and plugin will not process it


sl_zigbee_af_green_power_cluster_gp_notification_forward_cb#

bool sl_zigbee_af_green_power_cluster_gp_notification_forward_cb (uint16_t options, sl_zigbee_gp_address_t * addr, uint32_t gpdSecurityFrameCounter, uint8_t gpdCommandId, uint8_t * gpdCommandPayload, uint16_t gppShortAddress, uint8_t gppDistance)

Green Power Server notification forward callback.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]options

from the incoming Gp Notification Command

sl_zigbee_gp_address_t *[in]addr

GPD address

uint32_t[in]gpdSecurityFrameCounter

GPD Security Frame Counter

uint8_t[in]gpdCommandId

GPD Command ID

uint8_t *[in]gpdCommandPayload

GPD Command payload (first byte is length of the payload)

uint16_t[in]gppShortAddress

GPP Short Address

uint8_t[in]gppDistance

GPP Distance

This function is called by the Green Power Server plugin to notify the application of a Green Power Gp Notification of an incoming GPD command. Return true to handle in application.

Returns

  • True if application handled it and plugin will not process it anymore, else return False to process the notification by the plugin


sl_zigbee_af_green_power_server_gpd_commissioning_notification_cb#

bool sl_zigbee_af_green_power_server_gpd_commissioning_notification_cb (uint8_t commandId, uint16_t commNotificationOptions, sl_zigbee_gp_address_t * gpdAddr, uint32_t gpdSecurityFrameCounter, uint8_t gpdCommandId, uint8_t * gpdCommandPayload, uint16_t gppShortAddress, int8_t rssi, uint8_t linkQuality, uint8_t gppDistance, uint32_t commissioningNotificationMic)

Green Power Commissioning notification callback.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]commandId

Command ID

uint16_t[in]commNotificationOptions

Commissioning notification options

sl_zigbee_gp_address_t *[in]gpdAddr

GPD address

uint32_t[in]gpdSecurityFrameCounter

GPD Security Frame Counter

uint8_t[in]gpdCommandId

GPD Command ID

uint8_t *[in]gpdCommandPayload

GPD Command payload (first byte is length of the payload)

uint16_t[in]gppShortAddress

GPP Short Address

int8_t[in]rssi

RSSI

uint8_t[in]linkQuality

Link quality

uint8_t[in]gppDistance

GPP Distance

uint32_t[in]commissioningNotificationMic

MIC of commissioning notification

This function is called by the Green Power Server plugin to notify the application about Gp Commissioning notification received by the sink. If this function returns false indicating application does not handle the notification, the plugin will handle. If this returns true, the plugin will skip processing of the commissioning notification.

Returns

  • True if the user application wishes to consume the message and have the stack ignore the message, false otherwise, meaning the stack will process the GP Commissioning notification.


sl_zigbee_af_green_power_cluster_commissioning_message_status_notification_cb#

void sl_zigbee_af_green_power_cluster_commissioning_message_status_notification_cb (sl_zigbee_af_green_power_server_commissioning_state_t * commissioningState, sl_zigbee_aps_frame_t * apsFrame, sl_zigbee_outgoing_message_type_t messageType, uint16_t destination, sl_status_t status)

Sink commissioning enter call status notification callback.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_af_green_power_server_commissioning_state_t *[in]commissioningState

Sink commissioning state

sl_zigbee_aps_frame_t *[in]apsFrame

APS frame header

sl_zigbee_outgoing_message_type_t[in]messageType

Unicast or broadcast

uint16_t[in]destination

Destination node

sl_status_t[in]status

Status of the network submission

This function is called by the Green Power Server plugin from the sink commissioning enter command to notify the application of the status of the proxy commissioning enter message submission to network layer.


sl_zigbee_af_green_power_server_update_alias_cb#

bool sl_zigbee_af_green_power_server_update_alias_cb (sl_zigbee_gp_address_t * gpdAddr, uint16_t * alias)

Update alias information callback.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_gp_address_t *[in]gpdAddr

GPD address

uint16_t *[inout]alias

Alias

This function is called by the green power server plugin during commissioning to update alias information from user.

Returns

  • True if the alias is updated by the caller


sl_zigbee_af_green_power_server_pairing_status_cb#

void sl_zigbee_af_green_power_server_pairing_status_cb (sl_zigbee_sink_pairing_status_t status, sl_zigbee_commissioning_gpd_t * commissioningGpd)

Green Power Server pairing complete callback.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_sink_pairing_status_t[in]status

Status of the pairing

sl_zigbee_commissioning_gpd_t *[in]commissioningGpd

Context of the GPD that is currently commissioning

This function is called by the Green Power Server plugin during the pairing process to indicate the status. This may be called multiple times for a single pairing session. This provides the status as well as the current GPD context. This callback can be monitored to get information in case a GPD commissioning that has started ended up in success or failure. This callback does not give any information about a commissioning GPDF that gets filtered out earlier in the commissioning processing.


sl_zigbee_af_green_power_server_pre_sink_pairing_cb#

void sl_zigbee_af_green_power_server_pre_sink_pairing_cb (sl_zigbee_commissioning_gpd_t * commissioningGpd)

Green power server update sink list callback.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_commissioning_gpd_t *[in]commissioningGpd

Context of the GPD that is currently commissioning

This callback is called by the green power server at a final stage during pairing process. At this point the commissioning sink is ready to be saved or updated into the sink table and GpPairing announcement. This callback is helpful to supply or update the associated parameters to the sink entry. For example, a sink application can update a group list groupcast communication.