The information regarding scan results.

Public Attributes#

sl_status_t
int8_t
uint8_t
uint8_t
sl_zigbee_zigbee_network_t *
uint16_t

Public Attribute Documentation#

status#

sl_status_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::status

The status indicating the success or failure of a scan.

This member is only valid when sl_zigbee_af_scan_dispatch_scan_results_are_complete returns true.


rssi#

int8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::rssi

The RSSI found during a scan.

This member is only valid when sl_zigbee_af_scan_dispatch_scan_results_are_complete returns false.


channel#

uint8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::channel

The channel on which the scan is taking place.

This member is only valid when the results are for an energy scan or sl_zigbee_af_scan_dispatch_scan_results_are_complete returns true and sl_zigbee_af_scan_dispatch_scan_results_are_failure returns false. Note that in active scan results, users can find the channel on which the network was found using the network member of this structure.


lqi#

uint8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::lqi

The LQI found during the scan.

This member is only valid when the result are for an active scan.


network#

sl_zigbee_zigbee_network_t* sl_zigbee_af_plugin_scan_dispatch_scan_results_t::network

The Zigbee network found in the scan.

This member is only valid when the result are for an active scan.


mask#

uint16_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::mask

A mask containing information about the scan.