The include file for all the types for Ember ApplicationFramework.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_AF_API_TYPES
#define SILABS_AF_API_TYPES
#ifdef SL_COMPONENT_CATALOG_PRESENT
#include "sl_component_catalog.h"
#endif
#include "zap-type.h"
#include "app/framework/common/sl_zigbee_system_common.h"
#ifdef SL_CATALOG_ZIGBEE_MESSAGING_CLIENT_PRESENT
#include "messaging-client-config.h"
#endif // SL_CATALOG_ZIGBEE_MESSAGING_CLIENT_PRESENT
#ifdef EZSP_HOST
#include "app/util/ezsp/ezsp-enum.h"
#endif
typedef uint16_t sl_zigbee_af_profile_id_t;
typedef uint16_t sl_zigbee_af_attribute_id_t;
typedef uint16_t sl_zigbee_af_cluster_id_t;
typedef uint8_t sl_zigbee_af_attribute_type_t;
typedef uint8_t sl_zigbee_af_cluster_mask_t;
typedef uint8_t sl_zigbee_af_attribute_mask_t;
typedef void (*sl_zigbee_af_generic_cluster_function_t)(void);
typedef struct {
sl_zigbee_af_cluster_id_t clusterId;
sl_zigbee_af_cluster_mask_t functionMask;
const sl_zigbee_af_generic_cluster_function_t functionPtr;
} sli_cluster_function_structure_t;
#define SL_ZIGBEE_AF_NULL_MANUFACTURER_CODE 0x0000u
#define SL_ZIGBEE_AF_INVALID_PROFILE_ID 0xFFFFu
typedef union {
uint8_t *ptrToDefaultValue;
uint16_t defaultValue;
} sl_zigbee_af_default_attribute_value_t;
typedef struct {
sl_zigbee_af_default_attribute_value_t defaultValue;
sl_zigbee_af_default_attribute_value_t minValue;
sl_zigbee_af_default_attribute_value_t maxValue;
} sl_zigbee_af_attribute_min_max_value_t;
typedef union {
uint8_t *ptrToDefaultValue;
uint16_t defaultValue;
sl_zigbee_af_attribute_min_max_value_t *ptrToMinMaxValue;
} sl_zigbee_af_default_or_min_max_attribute_value_t;
typedef struct {
sl_zigbee_af_attribute_id_t attributeId;
sl_zigbee_af_attribute_type_t attributeType;
uint8_t size;
sl_zigbee_af_attribute_mask_t mask;
sl_zigbee_af_default_or_min_max_attribute_value_t defaultValue;
} sl_zigbee_af_attribute_metadata_t;
typedef struct {
sl_zigbee_af_cluster_id_t clusterId;
sl_zigbee_af_attribute_metadata_t *attributes;
uint16_t attributeCount;
uint16_t clusterSize;
sl_zigbee_af_cluster_mask_t mask;
const sl_zigbee_af_generic_cluster_function_t *functions;
} sl_zigbee_af_cluster_t;
typedef struct {
sl_zigbee_af_attribute_id_t zigbeeAttributeId;
sl_zigbee_af_attribute_id_t zigbeeMfgAttributeId;
sl_zigbee_af_attribute_type_t zigbeeAttributeType;
sl_zigbee_af_attribute_id_t matterAttributeId;
sl_zigbee_af_attribute_id_t matterMfgAttributeId;
sl_zigbee_af_attribute_type_t matterAttributeType;
} sl_zigbee_matter_af_multi_protocol_attribute_metadata_t;
typedef struct {
sl_zigbee_af_cluster_id_t zigbeeClusterId;
sl_zigbee_af_cluster_id_t zigbeeMfgClusterId;
sl_zigbee_af_cluster_id_t matterClusterId;
sl_zigbee_af_cluster_id_t matterMfgClusterId;
sl_zigbee_matter_af_multi_protocol_attribute_metadata_t *zigbeeMatterAttributeMap;
uint16_t clusterMappedAttributeCount;
} sl_zigbee_matter_af_multi_protocol_cluster_metadata_t;
typedef struct {
uint8_t endpoint;
sl_zigbee_af_cluster_id_t clusterId;
sl_zigbee_af_cluster_mask_t clusterMask;
sl_zigbee_af_attribute_id_t attributeId;
uint16_t manufacturerCode;
} sl_zigbee_af_attribute_search_record_t;
typedef struct {
uint16_t index;
uint16_t manufacturerCode;
} sl_zigbee_af_manufacturer_code_entry_t;
typedef uint64_t sl_zigbee_af_difference_type_t;
typedef struct {
sl_zigbee_incoming_message_type_t type;
sl_zigbee_aps_frame_t* apsFrame;
uint8_t* message;
uint16_t msgLen;
uint16_t source;
uint8_t lastHopLqi;
int8_t lastHopRssi;
uint8_t bindingTableIndex;
uint8_t addressTableIndex;
uint8_t networkIndex;
} sl_zigbee_af_incoming_message_t;
typedef uint8_t sl_zigbee_af_interpan_message_type_t;
#define SL_ZIGBEE_AF_INTER_PAN_UNICAST 0x00u
#define SL_ZIGBEE_AF_INTER_PAN_BROADCAST 0x08u
#define SL_ZIGBEE_AF_INTER_PAN_MULTICAST 0x0Cu
// Legacy names
#define INTER_PAN_UNICAST SL_ZIGBEE_AF_INTER_PAN_UNICAST
#define INTER_PAN_BROADCAST SL_ZIGBEE_AF_INTER_PAN_BROADCAST
#define INTER_PAN_MULTICAST SL_ZIGBEE_AF_INTER_PAN_MULTICAST
#define SL_ZIGBEE_AF_INTERPAN_OPTION_NONE 0x0000u
#define SL_ZIGBEE_AF_INTERPAN_OPTION_APS_ENCRYPT 0x0001u
#define SL_ZIGBEE_AF_INTERPAN_OPTION_MAC_HAS_LONG_ADDRESS 0x0002u
#define SL_ZIGBEE_AF_INTERPAN_OPTION_FRAGMENTATION 0x0004u // Extended FC Indicating Fragmentation
typedef uint16_t sl_zigbee_af_interpan_options_t;
typedef struct {
sl_zigbee_af_interpan_message_type_t messageType;
sl_802154_long_addr_t longAddress;
sl_802154_short_addr_t shortAddress;
sl_802154_pan_id_t panId;
sl_zigbee_af_profile_id_t profileId;
sl_zigbee_af_cluster_id_t clusterId;
sl_zigbee_multicast_id_t groupId;
sl_zigbee_af_interpan_options_t options;
} sl_zigbee_af_interpan_header_t;
// Legacy Name
#define sli_zigbee_interpan_header_t sl_zigbee_af_interpan_header_t
typedef uint8_t sl_zigbee_af_allowed_interpan_options_t;
#define SL_ZIGBEE_AF_INTERPAN_DIRECTION_CLIENT_TO_SERVER 0x01u
#define SL_ZIGBEE_AF_INTERPAN_DIRECTION_SERVER_TO_CLIENT 0x02u
#define SL_ZIGBEE_AF_INTERPAN_DIRECTION_BOTH 0x03u
#define SL_ZIGBEE_AF_INTERPAN_GLOBAL_COMMAND 0x04u
#define SL_ZIGBEE_AF_INTERPAN_MANUFACTURER_SPECIFIC 0x08u
typedef struct {
sl_zigbee_af_profile_id_t profileId;
sl_zigbee_af_cluster_id_t clusterId;
uint8_t commandId;
sl_zigbee_af_allowed_interpan_options_t options;
} sl_zigbee_af_allowed_inter_pan_message_t;
typedef struct {
sl_zigbee_aps_frame_t *apsFrame;
sl_zigbee_incoming_message_type_t type;
sl_802154_short_addr_t source;
uint8_t *buffer;
uint16_t bufLen;
bool clusterSpecific;
bool mfgSpecific;
uint16_t mfgCode;
uint8_t seqNum;
uint8_t commandId;
uint8_t payloadStartIndex;
uint8_t direction;
sl_zigbee_af_interpan_header_t *interPanHeader;
uint8_t networkIndex;
} sl_zigbee_af_cluster_command_t;
typedef struct {
sl_zigbee_af_cluster_t *cluster;
uint8_t clusterCount;
uint16_t endpointSize;
} sl_zigbee_af_endpoint_type_t;
#ifdef EZSP_HOST
typedef sl_zigbee_ezsp_decision_id_t sl_zigbee_af_tc_link_key_request_policy_t;
typedef sl_zigbee_ezsp_decision_id_t sl_zigbee_af_app_link_key_request_policy_t;
#define SL_ZIGBEE_AF_ALLOW_TC_KEY_REQUESTS SL_ZIGBEE_EZSP_ALLOW_TC_KEY_REQUESTS_AND_SEND_CURRENT_KEY
#define SL_ZIGBEE_AF_DENY_TC_KEY_REQUESTS SL_ZIGBEE_EZSP_DENY_TC_KEY_REQUESTS
#define SL_ZIGBEE_AF_ALLOW_APP_KEY_REQUESTS SL_ZIGBEE_EZSP_ALLOW_APP_KEY_REQUESTS
#define SL_ZIGBEE_AF_DENY_APP_KEY_REQUESTS SL_ZIGBEE_EZSP_DENY_APP_KEY_REQUESTS
#else
typedef sl_zigbee_tc_link_key_request_policy_t sl_zigbee_af_tc_link_key_request_policy_t;
typedef sl_zigbee_app_link_key_request_policy_t sl_zigbee_af_app_link_key_request_policy_t;
#define SL_ZIGBEE_AF_ALLOW_TC_KEY_REQUESTS SL_ZIGBEE_ALLOW_TC_LINK_KEY_REQUEST_AND_SEND_CURRENT_KEY
#define SL_ZIGBEE_AF_DENY_TC_KEY_REQUESTS SL_ZIGBEE_DENY_TC_LINK_KEY_REQUESTS
#define SL_ZIGBEE_AF_ALLOW_APP_KEY_REQUESTS SL_ZIGBEE_ALLOW_APP_LINK_KEY_REQUEST
#define SL_ZIGBEE_AF_DENY_APP_KEY_REQUESTS SL_ZIGBEE_DENY_APP_LINK_KEY_REQUESTS
#endif
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_security_profile_t
#else
typedef uint8_t sl_zigbee_af_security_profile_t;
enum
#endif
{
SL_ZIGBEE_AF_SECURITY_PROFILE_NONE = 0x00,
SL_ZIGBEE_AF_SECURITY_PROFILE_HA = 0x01,
SL_ZIGBEE_AF_SECURITY_PROFILE_HA12 = 0x02,
SL_ZIGBEE_AF_SECURITY_PROFILE_SE_TEST = 0x03,
SL_ZIGBEE_AF_SECURITY_PROFILE_SE_FULL = 0x04,
SL_ZIGBEE_AF_SECURITY_PROFILE_Z3 = 0x05,
SL_ZIGBEE_AF_SECURITY_PROFILE_Z4 = 0x06,
SL_ZIGBEE_AF_SECURITY_PROFILE_CUSTOM = 0xFF,
};
typedef struct {
sl_zigbee_af_security_profile_t securityProfile;
uint16_t tcBitmask;
sl_zigbee_extended_security_bitmask_t tcExtendedBitmask;
uint16_t nodeBitmask;
sl_zigbee_extended_security_bitmask_t nodeExtendedBitmask;
sl_zigbee_af_tc_link_key_request_policy_t tcLinkKeyRequestPolicy;
sl_zigbee_af_app_link_key_request_policy_t appLinkKeyRequestPolicy;
sl_zigbee_key_data_t preconfiguredKey;
} sl_zigbee_af_security_profile_data_t;
#ifndef DOXYGEN_SHOULD_SKIP_THIS
typedef struct {
sl_zigbee_node_type_t nodeType;
sl_zigbee_af_security_profile_t securityProfile;
} sli_zigbee_af_zigbee_pro_network;
#endif
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_endpoint_bitmask_t;
#else
typedef uint8_t sl_zigbee_af_endpoint_bitmask_t;
enum
#endif
{
SL_ZIGBEE_AF_ENDPOINT_DISABLED = 0x00,
SL_ZIGBEE_AF_ENDPOINT_ENABLED = 0x01,
};
typedef struct {
uint8_t endpoint;
sl_zigbee_af_profile_id_t profileId;
uint16_t deviceId;
uint8_t deviceVersion;
sl_zigbee_af_endpoint_type_t *endpointType;
uint8_t networkIndex;
sl_zigbee_af_endpoint_bitmask_t bitmask;
} sl_zigbee_af_defined_endpoint_t;
// Cluster-specific types
#if (SL_ZIGBEE_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 8)
typedef uint8_t sl_zigbee_af_plugin_esi_management_bitmask_t;
#elif (SL_ZIGBEE_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 16)
typedef uint16_t sl_zigbee_af_plugin_esi_management_bitmask_t;
#elif (SL_ZIGBEE_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 32)
typedef uint32_t sl_zigbee_af_plugin_esi_management_bitmask_t;
#else
#error "SL_ZIGBEE_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE cannot exceed 32"
#endif
typedef struct {
uint32_t eventId;
#if defined(EMBER_AF_PLUGIN_DRLC_SERVER) || defined(SL_CATALOG_ZIGBEE_DRLC_SERVER_PRESENT)
sl_802154_long_addr_t source;
uint8_t sourceEndpoint;
#endif //EMBER_AF_PLUGIN_DRLC_SERVER || SL_CATALOG_ZIGBEE_DRLC_SERVER_PRESENT
#if defined(EMBER_AF_PLUGIN_DRLC) || defined(SL_CATALOG_ZIGBEE_DRLC_PRESENT)
sl_zigbee_af_plugin_esi_management_bitmask_t esiBitmask;
#endif //EMBER_AF_PLUGIN_DRLC || SL_CATALOG_ZIGBEE_DRLC_PRESENT
uint8_t destinationEndpoint;
uint16_t deviceClass;
uint8_t utilityEnrollmentGroup;
uint32_t startTime;
uint16_t duration;
uint8_t criticalityLevel;
uint8_t coolingTempOffset;
uint8_t heatingTempOffset;
int16_t coolingTempSetPoint;
int16_t heatingTempSetPoint;
int8_t avgLoadPercentage;
uint8_t dutyCycle;
uint8_t eventControl;
uint32_t startRand;
uint32_t durationRand;
uint8_t optionControl;
} sl_zigbee_af_load_control_event_t;
typedef enum {
SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE = 0x00,
SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED = 0x01,
SL_ZIGBEE_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT = 0x02,
SL_ZIGBEE_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE = 0x03,
SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE = 0x04,
SL_ZIGBEE_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE = 0x05,
SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE = 0x06,
} sl_zigbee_af_service_discovery_status_t;
#define EM_AF_DISCOVERY_RESPONSE_MASK (0x05u)
#define sl_zigbee_af_have_discovery_response_status(status) ((status) & EM_AF_DISCOVERY_RESPONSE_MASK)
typedef struct {
sl_zigbee_af_service_discovery_status_t status;
uint16_t zdoRequestClusterId;
sl_802154_short_addr_t matchAddress;
const void* responseData;
} sl_zigbee_af_service_discovery_result_t;
typedef struct {
uint8_t count;
const uint8_t* list;
} sl_zigbee_af_endpoint_list_t;
typedef struct {
uint8_t inClusterCount;
const uint16_t* inClusterList;
uint8_t outClusterCount;
const uint16_t* outClusterList;
sl_zigbee_af_profile_id_t profileId;
uint16_t deviceId;
uint8_t endpoint;
} sl_zigbee_af_cluster_list_t;
typedef void (sl_zigbee_af_service_discovery_callback_t)(const sl_zigbee_af_service_discovery_result_t* result);
typedef void (sl_zigbee_af_partner_link_key_exchange_callback_t)(bool success);
typedef enum {
SL_ZIGBEE_AF_LONG_POLL,
SL_ZIGBEE_AF_SHORT_POLL,
} sl_zigbee_af_event_poll_control_t;
typedef enum {
SL_ZIGBEE_AF_OK_TO_SLEEP,
SL_ZIGBEE_AF_OK_TO_HIBERNATE = SL_ZIGBEE_AF_OK_TO_SLEEP,
SL_ZIGBEE_AF_OK_TO_NAP,
SL_ZIGBEE_AF_STAY_AWAKE,
} sl_zigbee_af_event_sleep_control_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_application_task_t
#else
typedef uint32_t sl_zigbee_af_application_task_t;
enum
#endif
{
// we may be able to remove these top two since they are
// handled by the stack on the SOC.
SL_ZIGBEE_AF_WAITING_FOR_DATA_ACK = 0x00000001, //not needed?
SL_ZIGBEE_AF_LAST_POLL_GOT_DATA = 0x00000002, //not needed?
SL_ZIGBEE_AF_WAITING_FOR_SERVICE_DISCOVERY = 0x00000004,
SL_ZIGBEE_AF_WAITING_FOR_ZDO_RESPONSE = 0x00000008,
SL_ZIGBEE_AF_WAITING_FOR_ZCL_RESPONSE = 0x00000010,
SL_ZIGBEE_AF_WAITING_FOR_REGISTRATION = 0x00000020,
SL_ZIGBEE_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE = 0x00000040,
SL_ZIGBEE_AF_FORCE_SHORT_POLL = 0x00000080,
SL_ZIGBEE_AF_FRAGMENTATION_IN_PROGRESS = 0x00000100,
SL_ZIGBEE_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY = 0x00000200,
SL_ZIGBEE_AF_WAITING_FOR_TC_KEY_UPDATE = 0x00000400,
};
typedef struct {
uint8_t endpoint;
sl_zigbee_af_cluster_id_t clusterId;
bool isClient;
sl_zigbee_af_event_poll_control_t pollControl;
sl_zigbee_af_event_sleep_control_t sleepControl;
sl_zigbee_event_control_t *eventControl;
} sl_zigbee_af_event_context;
// TODO: update doxygen
typedef struct {
uint8_t endpoint;
sl_zigbee_af_cluster_id_t clusterId;
bool isClient;
sl_zigbee_af_event_poll_control_t pollControl;
sl_zigbee_af_event_sleep_control_t sleepControl;
sli_zigbee_event_t *event;
} sl_zigbee_event_context_t;
typedef void (*sl_zigbee_af_network_event_handler_t)(void);
typedef void (*sl_zigbee_af_endpoint_event_handler_t)(uint8_t endpoint);
#define SL_ZIGBEE_AF_GROUP_TABLE_NULL_INDEX 0xFFu
#define SL_ZIGBEE_AF_GROUP_TABLE_UNUSED_ENDPOINT_ID 0x00u
#define ZCL_GROUPS_CLUSTER_MAXIMUM_NAME_LENGTH 16u
typedef struct {
uint8_t endpoint; // 0x00 when not in use
uint16_t groupId;
uint8_t bindingIndex;
#ifdef SL_ZIGBEE_AF_PLUGIN_GROUPS_SERVER_NAME_SUPPORT
uint8_t name[ZCL_GROUPS_CLUSTER_MAXIMUM_NAME_LENGTH + 1];
#endif
} sl_zigbee_af_group_table_entry_t;
#define SL_ZIGBEE_AF_SCENE_TABLE_NULL_INDEX 0xFFu
#define SL_ZIGBEE_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID 0x00u
#define ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH 16u
#define ZCL_SCENES_GLOBAL_SCENE_GROUP_ID 0x0000u
#define ZCL_SCENES_GLOBAL_SCENE_SCENE_ID 0x00u
// EMZIGBEE-6833: sl_zigbee_af_scene_table_entry_t declaration should be moved to the scenes component.
#ifdef SL_CATALOG_ZIGBEE_SCENES_PRESENT
#include "scenes-config.h"
#if (SL_ZIGBEE_AF_PLUGIN_SCENES_NAME_SUPPORT == 1)
#define SCENES_NAME_SUPPORT
#endif
#endif // SL_CATALOG_ZIGBEE_SCENES_PRESENT
typedef struct {
uint8_t endpoint; // 0x00 when this record is not in use
uint16_t groupId; // 0x0000 if not associated with a group
uint8_t sceneId;
#ifdef SCENES_NAME_SUPPORT
uint8_t name[ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH + 1];
#endif
uint16_t transitionTime; // in seconds
uint8_t transitionTime100ms; // in tenths of a seconds
#ifdef ZCL_USING_ON_OFF_CLUSTER_SERVER
bool hasOnOffValue;
bool onOffValue;
#endif
#ifdef ZCL_USING_LEVEL_CONTROL_CLUSTER_SERVER
bool hasCurrentLevelValue;
uint8_t currentLevelValue;
#endif
#ifdef ZCL_USING_THERMOSTAT_CLUSTER_SERVER
bool hasOccupiedCoolingSetpointValue;
int16_t occupiedCoolingSetpointValue;
bool hasOccupiedHeatingSetpointValue;
int16_t occupiedHeatingSetpointValue;
bool hasSystemModeValue;
uint8_t systemModeValue;
#endif
#ifdef ZCL_USING_COLOR_CONTROL_CLUSTER_SERVER
bool hasCurrentXValue;
uint16_t currentXValue;
bool hasCurrentYValue;
uint16_t currentYValue;
bool hasEnhancedCurrentHueValue;
uint16_t enhancedCurrentHueValue;
bool hasCurrentSaturationValue;
uint8_t currentSaturationValue;
bool hasColorLoopActiveValue;
uint8_t colorLoopActiveValue;
bool hasColorLoopDirectionValue;
uint8_t colorLoopDirectionValue;
bool hasColorLoopTimeValue;
uint16_t colorLoopTimeValue;
bool hasColorTemperatureMiredsValue;
uint16_t colorTemperatureMiredsValue;
#endif //ZCL_USING_COLOR_CONTROL_CLUSTER_SERVER
#ifdef ZCL_USING_DOOR_LOCK_CLUSTER_SERVER
bool hasLockStateValue;
uint8_t lockStateValue;
#endif
#ifdef ZCL_USING_WINDOW_COVERING_CLUSTER_SERVER
bool hasCurrentPositionLiftPercentageValue;
uint8_t currentPositionLiftPercentageValue;
bool hasCurrentPositionTiltPercentageValue;
uint8_t currentPositionTiltPercentageValue;
#endif
} sl_zigbee_af_scene_table_entry_t;
#if !defined(EMBER_AF_PLUGIN_MESSAGING_CLIENT) && !defined(SL_CATALOG_ZIGBEE_MESSAGING_CLIENT_PRESENT)
// To forward declare callbacks regardless of whether the plugin
// is enabled, define all data structures. To define
// the messaging client data struct, declare this variable.
#define SL_ZIGBEE_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE 0
#endif
typedef struct {
bool valid;
bool active;
sl_zigbee_af_plugin_esi_management_bitmask_t esiBitmask;
uint8_t clientEndpoint;
uint32_t messageId;
uint8_t messageControl;
uint32_t startTime;
uint32_t endTime;
uint16_t durationInMinutes;
uint8_t message[SL_ZIGBEE_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE + 1];
} sl_zigbee_af_plugin_messaging_client_message_t;
#define ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH 11u
typedef struct {
bool valid;
bool active;
uint8_t clientEndpoint;
uint32_t providerId;
uint8_t rateLabel[ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH + 1];
uint32_t issuerEventId;
uint32_t currentTime;
uint8_t unitOfMeasure;
uint16_t currency;
uint8_t priceTrailingDigitAndPriceTier;
uint8_t numberOfPriceTiersAndRegisterTier;
uint32_t startTime;
uint32_t endTime;
uint16_t durationInMinutes;
uint32_t price;
uint8_t priceRatio;
uint32_t generationPrice;
uint8_t generationPriceRatio;
uint32_t alternateCostDelivered;
uint8_t alternateCostUnit;
uint8_t alternateCostTrailingDigit;
uint8_t numberOfBlockThresholds;
uint8_t priceControl;
} sl_zigbee_af_plugin_price_client_price_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_plugin_price_cpp_auth_t
#else
typedef uint8_t sl_zigbee_af_plugin_price_cpp_auth_t;
enum
#endif
{
SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_PENDING = 0,
SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED = 1,
SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED = 2,
SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_FORCED = 3,
SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED = 4
};
#define SL_ZIGBEE_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID 0x00u
typedef struct {
sl_zigbee_af_reporting_direction_t direction;
uint8_t endpoint;
sl_zigbee_af_cluster_id_t clusterId;
sl_zigbee_af_attribute_id_t attributeId;
uint8_t mask;
uint16_t manufacturerCode;
union {
struct {
uint16_t minInterval;
uint16_t maxInterval;
uint32_t reportableChange;
} reported;
struct {
sl_802154_short_addr_t source;
uint8_t endpoint;
uint16_t timeout;
} received;
} data;
} sl_zigbee_af_plugin_reporting_entry_t;
typedef enum {
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS = 0x00,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_BUSY = 0x01,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS = 0x02,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED = 0x03,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED = 0x04,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED = 0xF9,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND = 0xFA,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL = 0xFB,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED = 0xFC,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED = 0xFD,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED = 0xFE,
SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT = 0xFF,
} sl_zigbee_af_plugin_tunneling_client_status_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_zll_commissioning_status_t
#else
typedef uint8_t sl_zigbee_af_zll_commissioning_status_t;
enum
#endif
{
SL_ZIGBEE_AF_ZLL_ABORTED_BY_APPLICATION = 0x00,
SL_ZIGBEE_AF_ZLL_CHANNEL_CHANGE_FAILED = 0x01,
SL_ZIGBEE_AF_ZLL_JOINING_FAILED = 0x02,
SL_ZIGBEE_AF_ZLL_NO_NETWORKS_FOUND = 0x03,
SL_ZIGBEE_AF_ZLL_PREEMPTED_BY_STACK = 0x04,
SL_ZIGBEE_AF_ZLL_SENDING_START_JOIN_FAILED = 0x05,
SL_ZIGBEE_AF_ZLL_SENDING_DEVICE_INFORMATION_REQUEST_FAILED = 0x06,
SL_ZIGBEE_AF_ZLL_SENDING_IDENTIFY_REQUEST_FAILED = 0x07,
SL_ZIGBEE_AF_ZLL_SENDING_RESET_TO_FACTORY_NEW_REQUEST_FAILED = 0x08,
SL_ZIGBEE_AF_ZLL_NETWORK_FORMATION_FAILED = 0x09,
SL_ZIGBEE_AF_ZLL_NETWORK_UPDATE_OPERATION = 0x0A,
};
typedef struct {
sl_zigbee_multicast_id_t groupId;
uint8_t groupType;
} sl_zigbee_af_plugin_zll_commissioning_group_information_record_t;
typedef struct {
sl_802154_short_addr_t networkAddress;
uint8_t endpointId;
uint16_t profileId;
uint16_t deviceId;
uint8_t version;
} sl_zigbee_af_plugin_zll_commissioning_endpoint_information_record_t;
typedef struct {
uint16_t manufacturerId;
uint16_t imageTypeId;
uint32_t firmwareVersion;
uint8_t deviceSpecificFileEui64[EUI64_SIZE];
} sl_zigbee_af_ota_image_id_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_image_block_request_options_t
#else
typedef uint8_t sl_zigbee_af_image_block_request_options_t;
enum
#endif
{
SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE = 0x00,
// Client supports Min Block Request field
SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT = 0x01,
// Server supports Min Block Request field
SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER = 0x02,
// The Image Block Request is actually simulated in place of an actually
// received Image Page Request
SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST = 0x04
};
typedef struct {
const sl_zigbee_af_ota_image_id_t* id;
uint32_t offset;
uint32_t waitTimeSecondsResponse;
sl_802154_short_addr_t source;
sl_802154_long_addr_t sourceEui; // optionally present in messages
// The minBlockRequestPeriod can be treated as milliseconds or seconds on the
// client. The OTA server plugin has optional support to probe clients and
// treat this field with appropriate units (ms or sec)
uint16_t minBlockRequestPeriod; // optionally present in messages
uint8_t maxDataSize;
uint8_t clientEndpoint;
sl_zigbee_af_image_block_request_options_t bitmask;
} sl_zigbee_af_image_block_request_callback_struct_t;
typedef enum {
SL_ZIGBEE_AF_OTA_STORAGE_SUCCESS = 0,
SL_ZIGBEE_AF_OTA_STORAGE_ERROR = 1,
SL_ZIGBEE_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG = 2,
SL_ZIGBEE_AF_OTA_STORAGE_PARTIAL_FILE_FOUND = 3,
SL_ZIGBEE_AF_OTA_STORAGE_OPERATION_IN_PROGRESS = 4,
} sl_zigbee_af_ota_storage_status_t;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_ota_download_result_t
#else
typedef uint8_t sl_zigbee_af_ota_download_result_t;
enum
#endif
{
SL_ZIGBEE_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS = 0,
SL_ZIGBEE_AF_OTA_DOWNLOAD_TIME_OUT = 1,
SL_ZIGBEE_AF_OTA_VERIFY_FAILED = 2,
SL_ZIGBEE_AF_OTA_SERVER_ABORTED = 3,
SL_ZIGBEE_AF_OTA_CLIENT_ABORTED = 4,
SL_ZIGBEE_AF_OTA_ERASE_FAILED = 5,
};
#define SL_ZIGBEE_AF_OTA_MAX_HEADER_STRING_LENGTH 32u
#define UID_SIZE 32u
typedef struct {
// Magic Number omitted since it is always the same.
uint16_t headerVersion;
uint16_t headerLength;
uint16_t fieldControl;
uint16_t manufacturerId;
uint16_t imageTypeId; // a.k.a. Device ID
uint32_t firmwareVersion;
uint16_t zigbeeStackVersion;
uint8_t headerString[SL_ZIGBEE_AF_OTA_MAX_HEADER_STRING_LENGTH + 1];
uint32_t imageSize;
uint8_t securityCredentials;
union {
uint8_t EUI64[EUI64_SIZE];
uint8_t UID[UID_SIZE];
} upgradeFileDestination;
uint16_t minimumHardwareVersion;
uint16_t maximumHardwareVersion;
} sl_zigbee_af_ota_header_t;
typedef struct {
uint16_t id;
uint32_t length;
} sl_zigbee_af_tag_data_t;
typedef enum {
NO_APP_MESSAGE = 0,
RECEIVED_PARTNER_CERTIFICATE = 1,
GENERATING_EPHEMERAL_KEYS = 2,
GENERATING_SHARED_SECRET = 3,
KEY_GENERATION_DONE = 4,
GENERATE_SHARED_SECRET_DONE = 5,
LINK_KEY_ESTABLISHED = 6,
NO_LOCAL_RESOURCES = 7,
PARTNER_NO_RESOURCES = 8,
TIMEOUT_OCCURRED = 9,
INVALID_APP_COMMAND = 10,
MESSAGE_SEND_FAILURE = 11,
PARTNER_SENT_TERMINATE = 12,
INVALID_PARTNER_MESSAGE = 13,
PARTNER_SENT_DEFAULT_RESPONSE_ERROR = 14,
BAD_CERTIFICATE_ISSUER = 15,
KEY_CONFIRM_FAILURE = 16,
BAD_KEY_ESTABLISHMENT_SUITE = 17,
KEY_TABLE_FULL = 18,
NO_ESTABLISHMENT_ALLOWED = 19,
/* 283k1 certificates need to have valid key usage.
*/
INVALID_CERTIFICATE_KEY_USAGE = 20,
} sl_zigbee_af_key_establishment_notify_message_t;
#define APP_NOTIFY_ERROR_CODE_START NO_LOCAL_RESOURCES
#define APP_NOTIFY_MESSAGE_TEXT { \
"None", \
"Received Cert", \
"Generate keys", \
"Generate secret", \
"Key generate done", \
"Generate secret done", \
"Link key verified", \
\
/* Transient Error codes */ \
"No local resources", \
"Partner no resources", \
"Timeout", \
"Invalid app. command", \
"Message send failure", \
"Partner sent terminate", \
"Bad message", \
"Partner sent Default Rsp", \
\
/* Fatal errors */ \
"Bad cert issuer", \
"Key confirm failure", \
"Bad key est. suite", \
"Key table full", \
"Not allowed", \
"Invalid Key Usage", \
}
typedef enum {
SL_ZIGBEE_AF_IMAGE_GOOD = 0,
SL_ZIGBEE_AF_IMAGE_BAD = 1,
SL_ZIGBEE_AF_IMAGE_VERIFY_IN_PROGRESS = 2,
#ifndef DOXYGEN_SHOULD_SKIP_THIS
// Internal use only.
SL_ZIGBEE_AF_IMAGE_VERIFY_WAIT = 3,
SL_ZIGBEE_AF_IMAGE_VERIFY_ERROR = 4,
SL_ZIGBEE_AF_IMAGE_UNKNOWN = 5,
SL_ZIGBEE_AF_NO_IMAGE_VERIFY_SUPPORT = 6,
#endif
} sl_zigbee_af_image_verify_status_t;
typedef void (*sl_zigbee_af_tick_function_t)(uint8_t endpoint);
typedef void (*sl_zigbee_af_init_function_t)(uint8_t endpoint);
typedef void (*sl_zigbee_af_cluster_attribute_changed_callback_t)(uint8_t endpoint,
sl_zigbee_af_attribute_id_t attributeId);
typedef void (*sl_zigbee_af_manufacturer_specific_cluster_attribute_changed_callback_t)(uint8_t endpoint,
sl_zigbee_af_attribute_id_t attributeId,
uint16_t manufacturerCode);
typedef sl_zigbee_af_status_t (*sl_zigbee_af_cluster_pre_attribute_changed_callback_t)(uint8_t endpoint,
sl_zigbee_af_attribute_id_t attributeId,
sl_zigbee_af_attribute_type_t attributeType,
uint8_t size,
uint8_t *value);
typedef void (*sl_zigbee_af_default_response_function_t)(uint8_t endpoint,
uint8_t commandId,
sl_zigbee_af_status_t status);
typedef void (*sl_zigbee_af_message_sent_function_t)(sl_zigbee_outgoing_message_type_t type,
uint16_t indexOrDestination,
sl_zigbee_aps_frame_t *apsFrame,
uint16_t msgLen,
uint8_t *message,
sl_status_t status);
typedef struct {
sl_zigbee_af_message_sent_function_t callback;
sl_zigbee_aps_frame_t* apsFrame;
uint8_t* message;
uint16_t indexOrDestination;
uint16_t messageLength;
sl_zigbee_outgoing_message_type_t type;
bool broadcast;
} sl_zigbee_af_message_struct_t;
typedef struct {
sl_802154_long_addr_t deviceId;
sl_zigbee_key_data_t key;
} sl_zigbee_af_link_key_backup_data_t;
typedef struct {
sl_802154_long_addr_t extendedPanId;
uint8_t keyListLength;
uint8_t maxKeyListLength;
sl_zigbee_af_link_key_backup_data_t* keyList;
} sl_zigbee_af_trust_center_backup_data_t;
#define SL_ZIGBEE_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH 16u
typedef struct {
uint8_t hardwareTag[SL_ZIGBEE_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH];
uint8_t eui64[EUI64_SIZE];
uint16_t mfgId;
uint16_t bootloaderVersion;
uint8_t capabilities;
uint8_t platform;
uint8_t micro;
uint8_t phy;
bool bootloaderActive;
} sl_zigbee_af_standalone_bootloader_query_response_data_t;
typedef struct {
uint16_t clusterId;
uint8_t commandId;
uint8_t mask;
} sl_zigbee_af_command_metadata_t;
typedef struct {
uint16_t year;
uint8_t month;
uint8_t day;
uint8_t hours;
uint8_t minutes;
uint8_t seconds;
} sl_zigbee_af_time_struct_t;
typedef struct {
uint8_t year;
uint8_t month;
uint8_t dayOfMonth;
uint8_t dayOfWeek;
} sl_zigbee_af_date_t;
/* Simple Metering Server Test Code */
#define SL_ZIGBEE_AF_PLUGIN_SIMPLE_METERING_SERVER_ELECTRIC_METER 0
#define SL_ZIGBEE_AF_PLUGIN_SIMPLE_METERING_SERVER_GAS_METER 1
// Functional Notification Flags
// Also #defined in enums.h under slightly different names
#define SL_ZIGBEE_AF_METERING_FNF_NEW_OTA_FIRMWARE 0x00000001
#define SL_ZIGBEE_AF_METERING_FNF_CBKE_UPDATE_REQUEST 0x00000002
#define SL_ZIGBEE_AF_METERING_FNF_TIME_SYNC 0x00000004
#define SL_ZIGBEE_AF_METERING_FNF_STAY_AWAKE_REQUEST_HAN 0x00000010
#define SL_ZIGBEE_AF_METERING_FNF_STAY_AWAKE_REQUEST_WAN 0x00000020
#define SL_ZIGBEE_AF_METERING_FNF_PUSH_HISTORICAL_METERING_DATA_ATTRIBUTE_SET 0x000001C0
#define SL_ZIGBEE_AF_METERING_FNF_PUSH_HISTORICAL_PREPAYMENT_DATA_ATTRIBUTE_SET 0x00000E00
#define SL_ZIGBEE_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_BASIC_CLUSTER 0x00001000
#define SL_ZIGBEE_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_METERING_CLUSTER 0x00002000
#define SL_ZIGBEE_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_PREPAYMENT_CLUSTER 0x00004000
#define SL_ZIGBEE_AF_METERING_FNF_NETWORK_KEY_ACTIVE 0x00008000
#define SL_ZIGBEE_AF_METERING_FNF_DISPLAY_MESSAGE 0x00010000
#define SL_ZIGBEE_AF_METERING_FNF_CANCEL_ALL_MESSAGES 0x00020000
#define SL_ZIGBEE_AF_METERING_FNF_CHANGE_SUPPLY 0x00040000
#define SL_ZIGBEE_AF_METERING_FNF_LOCAL_CHANGE_SUPPLY 0x00080000
#define SL_ZIGBEE_AF_METERING_FNF_SET_UNCONTROLLED_FLOW_THRESHOLD 0x00100000
#define SL_ZIGBEE_AF_METERING_FNF_TUNNEL_MESSAGE_PENDING 0x00200000
#define SL_ZIGBEE_AF_METERING_FNF_GET_SNAPSHOT 0x00400000
#define SL_ZIGBEE_AF_METERING_FNF_GET_SAMPLED_DATA 0x00800000
#define SL_ZIGBEE_AF_METERING_FNF_NEW_SUB_GHZ_CHANNEL_MASKS_AVAILABLE 0x01000000
#define SL_ZIGBEE_AF_METERING_FNF_ENERGY_SCAN_PENDING 0x02000000
#define SL_ZIGBEE_AF_METERING_FNF_CHANNEL_CHANGE_PENDING 0x04000000
// Notification Flags 2
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_PRICE 0x00000001
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_BLOCK_PERIOD 0x00000002
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_TARIFF_INFORMATION 0x00000004
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_CONVERSION_FACTOR 0x00000008
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_CALORIFIC_VALUE 0x00000010
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_CO2_VALUE 0x00000020
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_BILLING_PERIOD 0x00000040
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_CONSOLIDATED_BILL 0x00000080
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_PRICE_MATRIX 0x00000100
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_BLOCK_THRESHOLDS 0x00000200
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_CURRENCY_CONVERSION 0x00000400
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_CREDIT_PAYMENT_INFO 0x00001000
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_CPP_EVENT 0x00002000
#define SL_ZIGBEE_AF_METERING_NF2_PUBLISH_TIER_LABELS 0x00004000
#define SL_ZIGBEE_AF_METERING_NF2_CANCEL_TARIFF 0x00008000
// Notification Flags 3
#define SL_ZIGBEE_AF_METERING_NF3_PUBLISH_CALENDAR 0x00000001
#define SL_ZIGBEE_AF_METERING_NF3_PUBLISH_SPECIAL_DAYS 0x00000002
#define SL_ZIGBEE_AF_METERING_NF3_PUBLISH_SEASONS 0x00000004
#define SL_ZIGBEE_AF_METERING_NF3_PUBLISH_WEEK 0x00000008
#define SL_ZIGBEE_AF_METERING_NF3_PUBLISH_DAY 0x00000010
#define SL_ZIGBEE_AF_METERING_NF3_CANCEL_CALENDAR 0x00000020
// Notification Flags 4
#define SL_ZIGBEE_AF_METERING_NF4_SELECT_AVAILABLE_EMERGENCY_CREDIT 0x00000001
#define SL_ZIGBEE_AF_METERING_NF4_CHANGE_DEBT 0x00000002
#define SL_ZIGBEE_AF_METERING_NF4_EMERGENCY_CREDIT_SETUP 0x00000004
#define SL_ZIGBEE_AF_METERING_NF4_CONSUMER_TOP_UP 0x00000008
#define SL_ZIGBEE_AF_METERING_NF4_CREDIT_ADJUSTMENT 0x00000010
#define SL_ZIGBEE_AF_METERING_NF4_CHANGE_PAYMENT_MODE 0x00000020
#define SL_ZIGBEE_AF_METERING_NF4_GET_PREPAY_SNAPSHOT 0x00000040
#define SL_ZIGBEE_AF_METERING_NF4_GET_TOP_UP_LOG 0x00000080
#define SL_ZIGBEE_AF_METERING_NF4_SET_LOW_CREDIT_WARNING_LEVEL 0x00000100
#define SL_ZIGBEE_AF_METERING_NF4_GET_DEBT_REPAYMENT_LOG 0x00000200
#define SL_ZIGBEE_AF_METERING_NF4_SET_MAXIMUM_CREDIT_LIMIT 0x00000400
#define SL_ZIGBEE_AF_METERING_NF4_SET_OVERALL_DEBT_CAP 0x00000800
// Notification Flags 5
#define SL_ZIGBEE_AF_METERING_NF5_PUBLISH_CHANGE_OF_TENANCY 0x00000001
#define SL_ZIGBEE_AF_METERING_NF5_PUBLISH_CHANGE_OF_SUPPLIER 0x00000002
#define SL_ZIGBEE_AF_METERING_NF5_REQUEST_NEW_PASSWORD_1_RESPONSE 0x00000004
#define SL_ZIGBEE_AF_METERING_NF5_REQUEST_NEW_PASSWORD_2_RESPONSE 0x00000008
#define SL_ZIGBEE_AF_METERING_NF5_REQUEST_NEW_PASSWORD_3_RESPONSE 0x00000010
#define SL_ZIGBEE_AF_METERING_NF5_REQUEST_NEW_PASSWORD_4_RESPONSE 0x00000020
#define SL_ZIGBEE_AF_METERING_NF5_UPDATE_SITE_ID 0x00000040
#define SL_ZIGBEE_AF_METERING_NF5_RESET_BATTERY_COUNTER 0x00000080
#define SL_ZIGBEE_AF_METERING_NF5_UPDATE_CIN 0x00000100
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_cbke_key_establishment_suite_t
#else
typedef uint16_t sl_zigbee_af_cbke_key_establishment_suite_t;
enum
#endif
{
SL_ZIGBEE_AF_INVALID_KEY_ESTABLISHMENT_SUITE = 0x0000,
SL_ZIGBEE_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1 = 0x0001,
SL_ZIGBEE_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1 = 0x0002,
};
#define SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH (16u)
#define SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH (18u)
#define SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH (32u)
#define SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH (24u)
#define SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH (10u)
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_device_management_password_type_t
#else
typedef uint16_t sl_zigbee_af_device_management_password_type_t;
enum
#endif
{
UNUSED_PASSWORD = 0x00,
SERVICE_PASSWORD = 0x01,
CONSUMER_PASSWORD = 0x02,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum sl_zigbee_af_device_management_change_pending_flags_t
#else
typedef uint8_t sl_zigbee_af_device_management_change_pending_flags_t;
enum
#endif
{
SL_ZIGBEE_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK = 0x01,
SL_ZIGBEE_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK = 0x02,
SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK = 0x04,
SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK = 0x08,
SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK = 0x10,
SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK = 0x20,
};
typedef struct {
// Optional fields only used by Gas Proxy Function plugin.
uint32_t providerId;
uint32_t issuerEventId;
uint8_t tariffType;
// always used fields
uint32_t implementationDateTime;
uint32_t tenancy;
} sl_zigbee_af_device_management_tenancy_t;
typedef struct {
uint32_t proposedProviderId;
uint32_t implementationDateTime;
uint32_t providerChangeControl;
uint8_t proposedProviderName[SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH + 1];
uint8_t proposedProviderContactDetails[SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH + 1];
} sl_zigbee_af_device_management_supplier_t;
typedef struct {
uint32_t requestDateTime;
uint32_t implementationDateTime;
uint8_t supplyStatus;
uint8_t originatorIdSupplyControlBits;
} sl_zigbee_af_device_management_supply_t;
typedef struct {
uint8_t siteId[SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH + 1];
uint32_t implementationDateTime;
uint32_t issuerEventId;
} sl_zigbee_af_device_management_site_id_t;
typedef struct {
uint8_t cin[SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH + 1];
uint32_t implementationDateTime;
uint32_t issuerEventId;
} sl_zigbee_af_device_management_c_i_n_t;
typedef struct {
bool supplyTamperState;
bool supplyDepletionState;
bool supplyUncontrolledFlowState;
bool loadLimitSupplyState;
} sl_zigbee_af_device_management_supply_status_flags_t;
typedef struct {
uint16_t uncontrolledFlowThreshold;
uint16_t multiplier;
uint16_t divisor;
uint16_t measurementPeriod;
uint8_t unitOfMeasure;
uint8_t stabilisationPeriod;
} sl_zigbee_af_device_management_uncontrolled_flow_threshold_t;
typedef struct {
uint32_t implementationDateTime;
uint8_t supplyStatus;
} sl_zigbee_af_device_management_supply_status_t;
typedef struct {
uint8_t password[SL_ZIGBEE_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH + 1];
uint32_t implementationDateTime;
uint16_t durationInMinutes;
sl_zigbee_af_device_management_password_type_t passwordType;
} sl_zigbee_af_device_management_password_t;
typedef struct {
sl_zigbee_af_device_management_tenancy_t tenancy;
sl_zigbee_af_device_management_supplier_t supplier;
sl_zigbee_af_device_management_supply_t supply;
sl_zigbee_af_device_management_site_id_t siteId;
sl_zigbee_af_device_management_c_i_n_t cin;
sl_zigbee_af_device_management_supply_status_flags_t supplyStatusFlags;
sl_zigbee_af_device_management_supply_status_t supplyStatus;
//TODO: These passwords ought to be tokenized / hashed
sl_zigbee_af_device_management_password_t servicePassword;
sl_zigbee_af_device_management_password_t consumerPassword;
sl_zigbee_af_device_management_uncontrolled_flow_threshold_t threshold;
uint32_t providerId;
uint32_t issuerEventId;
uint8_t proposedLocalSupplyStatus;
sl_zigbee_af_tariff_type_t tariffType;
sl_zigbee_af_device_management_change_pending_flags_t pendingUpdates;
} sl_zigbee_af_device_management_info_t;
typedef struct {
uint8_t startIndex;
uint8_t endIndex;
} sl_zigbee_af_device_management_attribute_range_t;
// attrRange is a list of attributeId values in a cluster. It's needed to track contiguous
// segments of valid attributeId's with gaps in the middle.
// attributeSetId is the value of the upper byte in the attributeId. It ranges from 0x01(Price)
// to 0x08(OTA Event Configuration)
// Eg. {0x00,0x05} and {0x08,0x0A}
// We're betting that there isn't a list of cluster attributes that has more than 5 gaps.
typedef struct {
uint8_t attributeSetId;
sl_zigbee_af_device_management_attribute_range_t attributeRange[7];
} sl_zigbee_af_device_management_attribute_table_t;
typedef struct {
bool encryption;
uint8_t * plainPayload;
uint16_t plainPayloadLength;
uint8_t * encryptedPayload;
uint16_t encryptedPayloadLength;
} sl_zigbee_af_gbz_message_data_t;
typedef struct {
uint8_t * gbzCommands;
uint16_t gbzCommandsLength;
uint8_t * gbzCommandsResponse;
uint16_t gbzCommandsResponseLength;
uint16_t messageCode;
} sl_zigbee_af_gpf_message_t;
typedef uint16_t sl_zigbee_af_remote_cluster_type_t;
#define SL_ZIGBEE_AF_REMOTE_CLUSTER_TYPE_NONE 0x0000u
#define SL_ZIGBEE_AF_REMOTE_CLUSTER_TYPE_SERVER 0x0001u
#define SL_ZIGBEE_AF_REMOTE_CLUSTER_TYPE_CLIENT 0x0002u
#define SL_ZIGBEE_AF_REMOTE_CLUSTER_TYPE_INVALID 0xFFFFu
typedef struct {
sl_zigbee_af_cluster_id_t clusterId;
sl_zigbee_af_profile_id_t profileId;
uint16_t deviceId;
uint8_t endpoint;
sl_zigbee_af_remote_cluster_type_t type;
} sl_zigbee_af_remote_cluster_struct_t;
typedef struct {
sl_802154_long_addr_t targetEUI64;
uint8_t sourceEndpoint;
uint8_t destEndpoint;
uint16_t clusterId;
sl_802154_long_addr_t destEUI64;
sl_802154_long_addr_t sourceEUI64;
} sl_zigbee_af_remote_binding_struct_t;
typedef struct {
sl_zigbee_af_cluster_id_t clusterId;
bool server;
} sl_zigbee_af_cluster_info_t;
#ifdef SL_CATALOG_ZIGBEE_DEVICE_DATABASE_PRESENT
#include "device-database-config.h"
#else
#define SL_ZIGBEE_AF_MAX_CLUSTERS_PER_ENDPOINT 3u
#define SL_ZIGBEE_AF_MAX_ENDPOINTS_PER_DEVICE 1u
#endif
typedef struct {
sl_zigbee_af_cluster_info_t clusters[SL_ZIGBEE_AF_MAX_CLUSTERS_PER_ENDPOINT];
sl_zigbee_af_profile_id_t profileId;
uint16_t deviceId;
uint8_t endpoint;
uint8_t clusterCount;
} sl_zigbee_af_endpoint_info_struct_t;
// Although we treat this like a bitmap, only 1 bit is set at a time.
// We use the bitmap feature to allow us to find all devices
// with any in a set of status codes using
// sl_zigbee_af_device_database_find_device_by_status().
typedef enum {
SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_NONE = 0x00,
SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_NEW = 0x01,
SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS = 0x02,
SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS = 0x04,
SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION = 0x08,
SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_DONE = 0x40,
SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FAILED = 0x80,
} sl_zigbee_af_device_discovery_status_t;
typedef struct {
sl_802154_long_addr_t eui64;
sl_zigbee_af_endpoint_info_struct_t endpoints[SL_ZIGBEE_AF_MAX_ENDPOINTS_PER_DEVICE];
sl_zigbee_af_device_discovery_status_t status;
uint8_t discoveryFailures;
uint8_t capabilities;
uint8_t endpointCount;
uint8_t stackRevision;
} sl_zigbee_af_device_info_t;
typedef struct {
uint16_t deviceIndex;
} sl_zigbee_af_device_database_iterator_t;
typedef struct {
sl_802154_short_addr_t sl_zigbee_node_id;
uint32_t timeStamp;
} sl_zigbee_af_joining_device_t;
#define SL_ZIGBEE_AF_INVALID_CLUSTER_ID 0xFFFFu
#define SL_ZIGBEE_AF_INVALID_ENDPOINT 0xFFu
#define SL_ZIGBEE_AF_INVALID_ENDPOINT_INDEX 0xFFu
#define SL_ZIGBEE_AF_INVALID_PAN_ID 0xFFFFu
#define SL_ZIGBEE_AF_PERMIT_JOIN_FOREVER 0xFFu
#define SL_ZIGBEE_AF_PERMIT_JOIN_MAX_TIMEOUT 0xFEu
#define SL_ZIGBEE_AF_ZDO_RESPONSE_OVERHEAD 2u
typedef uint32_t sl_zigbee_af_zcl_request_status_t;
#define SL_ZIGBEE_ZCL_STATUS_INTERNAL_COMMAND_HANDLED 0xFFFFFF00u
#endif // SILABS_AF_API_TYPES
Modules#
sli_cluster_function_structure_t
sl_zigbee_af_default_attribute_value_t
sl_zigbee_af_attribute_min_max_value_t
sl_zigbee_af_default_or_min_max_attribute_value_t
sl_zigbee_af_attribute_metadata_t
sl_zigbee_matter_af_multi_protocol_attribute_metadata_t
sl_zigbee_matter_af_multi_protocol_cluster_metadata_t
sl_zigbee_af_attribute_search_record_t
sl_zigbee_af_manufacturer_code_entry_t
sl_zigbee_af_incoming_message_t
sl_zigbee_af_interpan_header_t
sl_zigbee_af_allowed_inter_pan_message_t
sl_zigbee_af_cluster_command_t
sl_zigbee_af_security_profile_data_t
sl_zigbee_af_defined_endpoint_t
sl_zigbee_af_load_control_event_t
sl_zigbee_af_service_discovery_result_t
sl_zigbee_af_group_table_entry_t
sl_zigbee_af_scene_table_entry_t
sl_zigbee_af_plugin_messaging_client_message_t
sl_zigbee_af_plugin_price_client_price_t
sl_zigbee_af_plugin_reporting_entry_t
sl_zigbee_af_plugin_zll_commissioning_group_information_record_t
sl_zigbee_af_plugin_zll_commissioning_endpoint_information_record_t
sl_zigbee_af_image_block_request_callback_struct_t
sl_zigbee_af_link_key_backup_data_t
sl_zigbee_af_trust_center_backup_data_t
sl_zigbee_af_standalone_bootloader_query_response_data_t
sl_zigbee_af_command_metadata_t
sl_zigbee_af_device_management_tenancy_t
sl_zigbee_af_device_management_supplier_t
sl_zigbee_af_device_management_supply_t
sl_zigbee_af_device_management_site_id_t
sl_zigbee_af_device_management_c_i_n_t
sl_zigbee_af_device_management_supply_status_flags_t
sl_zigbee_af_device_management_uncontrolled_flow_threshold_t
sl_zigbee_af_device_management_supply_status_t
sl_zigbee_af_device_management_password_t
sl_zigbee_af_device_management_info_t
sl_zigbee_af_device_management_attribute_range_t
sl_zigbee_af_device_management_attribute_table_t
sl_zigbee_af_gbz_message_data_t
sl_zigbee_af_remote_cluster_struct_t
sl_zigbee_af_remote_binding_struct_t
sl_zigbee_af_endpoint_info_struct_t
sl_zigbee_af_device_database_iterator_t
Macros#
A distinguished manufacturer code that is used to indicate the absence of a manufacturer-specific profile, cluster, command, or attribute.
An invalid profile ID This is a reserved profileId.
A simple way to determine if the service discovery callback has a response.
Indicate the absence of a Group table entry.
Value used when setting or getting the endpoint in a Group table entry. It indicates that the entry is not in use.
Maximum length of Group names, not including the length byte.
Indicates the absence of a Scene table entry.
Value used when setting or getting the endpoint in a Scene table entry. It indicates that the entry is not in use.
Maximum length of Scene names, not including the length byte.
The group identifier for the global scene.
The scene identifier for the global scene.
Use when setting or getting the endpoint in a report table entry. It indicates that the entry is not in use.
The maximum size of the string that is present in the header of the Zigbee Over-the-air file format.
The length of the hardware tag in the Ember Bootloader Query Response.
Device Management plugin types.
Permit join times.
The overhead of the ZDO response. 1 byte for the sequence and 1 byte for the status code.
ZCL request handler status indicates a command was handled and no default response should be sent.
Enumerations#
Indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.
Control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For example, if two events are active, one with SL_ZIGBEE_AF_LONG_POLL and the other with SL_ZIGBEE_AF_SHORT_POLL, the processor will short poll until the second event is deactivated.
Control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For example, if two events are active, one with SL_ZIGBEE_AF_OK_TO_HIBERNATE and the other with SL_ZIGBEE_AF_OK_TO_NAP, the processor will only be allowed to sleep until the second event is deactivated.
Track tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ACK, the application needs to stay out of hibernation to wait and poll for it.
Specifies CPP Authorization values.
Status codes used by the ZLL Commissioning plugin.
The list of options possible for the image block request/response.
Contain the success or error code of an OTA storage device operation.
Contain the success or error code of an OTA download operation.
Indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer-specific verification.
CBKE Library types.
Typedefs#
Refer to the Zigbee application profile ID.
Refer to the ZCL attribute ID.
Refer to the ZCL cluster ID.
Refer to the ZCL attribute type.
User for the cluster mask.
User for the attribute mask.
Use for either of the cluster functions.
Interpan Message type: unicast, broadcast, or multicast.
The options for sending/receiving interpan messages.
The options for what interpan messages are allowed.
Bitmask data type for storing one bit of information for each ESI in the ESI table.
Define a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, the callback is only fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast, multiple callbacks may be fired with SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a few seconds, the callback is fired with SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.
Define a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.
Refer to the handler for network events.
Refer to the handler for endpoint events.
Refer to the tick callback for cluster.
Refer to the init callback for cluster.
Refer to the attribute changed callback function.
Refer to the manufacturer-specific attribute changed callback function.
Refer to the pre-attribute changed callback function.
Refer to the default response callback function.
Refer to the message sent callback function.
Zigbee Internet Client/Server Remote Cluster Types.
return status for cluster request handlers - may be `sl_zigbee_af_status_t` or a special return status indicate special handling of the response by the request handler
Enumeration Documentation#
sl_zigbee_af_security_profile_t#
sl_zigbee_af_security_profile_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_SECURITY_PROFILE_NONE | |
| SL_ZIGBEE_AF_SECURITY_PROFILE_HA | |
| SL_ZIGBEE_AF_SECURITY_PROFILE_HA12 | |
| SL_ZIGBEE_AF_SECURITY_PROFILE_SE_TEST | |
| SL_ZIGBEE_AF_SECURITY_PROFILE_SE_FULL | |
| SL_ZIGBEE_AF_SECURITY_PROFILE_Z3 | |
| SL_ZIGBEE_AF_SECURITY_PROFILE_Z4 | |
| SL_ZIGBEE_AF_SECURITY_PROFILE_CUSTOM | |
sl_zigbee_af_service_discovery_status_t#
sl_zigbee_af_service_discovery_status_t
Indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE | |
| SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED | |
| SL_ZIGBEE_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT | |
| SL_ZIGBEE_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE | |
| SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE | |
| SL_ZIGBEE_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE | |
| SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE | |
sl_zigbee_af_event_poll_control_t#
sl_zigbee_af_event_poll_control_t
Control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For example, if two events are active, one with SL_ZIGBEE_AF_LONG_POLL and the other with SL_ZIGBEE_AF_SHORT_POLL, the processor will short poll until the second event is deactivated.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_LONG_POLL | |
| SL_ZIGBEE_AF_SHORT_POLL | |
sl_zigbee_af_event_sleep_control_t#
sl_zigbee_af_event_sleep_control_t
Control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For example, if two events are active, one with SL_ZIGBEE_AF_OK_TO_HIBERNATE and the other with SL_ZIGBEE_AF_OK_TO_NAP, the processor will only be allowed to sleep until the second event is deactivated.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_OK_TO_SLEEP | |
| SL_ZIGBEE_AF_OK_TO_HIBERNATE | Deprecated |
| SL_ZIGBEE_AF_OK_TO_NAP | Deprecated |
| SL_ZIGBEE_AF_STAY_AWAKE | |
sl_zigbee_af_application_task_t#
sl_zigbee_af_application_task_t
Track tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ACK, the application needs to stay out of hibernation to wait and poll for it.
Some tasks do not necessarily have a response. For example, a ZDO request may or may not have a response. In this case, the application framework cannot rely on the fact that a response will come in to end the wake cycle, so the Application framework must time out the wake cycle if no expected response is received or no other event can be relied upon to end the wake cycle.
Add these types of tasks to the wake timeout mask by calling sl_zigbee_af_set_wake_timeout_bitmask_cb so that they can be governed by a timeout instead of a request / response.
The current tasks bitmask is an uint32_t bitmask used to track which tasks are active at any given time. The bottom 16 bits, values 0x01 - 0x8000 are reserved for Ember's use. The top 16 bits are reserved for the customer, values 0x10000 - 0x80000000
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_WAITING_FOR_DATA_ACK | |
| SL_ZIGBEE_AF_LAST_POLL_GOT_DATA | |
| SL_ZIGBEE_AF_WAITING_FOR_SERVICE_DISCOVERY | |
| SL_ZIGBEE_AF_WAITING_FOR_ZDO_RESPONSE | |
| SL_ZIGBEE_AF_WAITING_FOR_ZCL_RESPONSE | |
| SL_ZIGBEE_AF_WAITING_FOR_REGISTRATION | |
| SL_ZIGBEE_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE | |
| SL_ZIGBEE_AF_FORCE_SHORT_POLL | |
| SL_ZIGBEE_AF_FRAGMENTATION_IN_PROGRESS | |
| SL_ZIGBEE_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY | |
| SL_ZIGBEE_AF_WAITING_FOR_TC_KEY_UPDATE | |
sl_zigbee_af_plugin_price_cpp_auth_t#
sl_zigbee_af_plugin_price_cpp_auth_t
Specifies CPP Authorization values.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_PENDING | |
| SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED | |
| SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED | |
| SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_FORCED | |
| SL_ZIGBEE_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED | |
sl_zigbee_af_plugin_tunneling_client_status_t#
sl_zigbee_af_plugin_tunneling_client_status_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_BUSY | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED | |
| SL_ZIGBEE_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT | |
sl_zigbee_af_zll_commissioning_status_t#
sl_zigbee_af_zll_commissioning_status_t
Status codes used by the ZLL Commissioning plugin.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_ZLL_ABORTED_BY_APPLICATION | |
| SL_ZIGBEE_AF_ZLL_CHANNEL_CHANGE_FAILED | |
| SL_ZIGBEE_AF_ZLL_JOINING_FAILED | |
| SL_ZIGBEE_AF_ZLL_NO_NETWORKS_FOUND | |
| SL_ZIGBEE_AF_ZLL_PREEMPTED_BY_STACK | |
| SL_ZIGBEE_AF_ZLL_SENDING_START_JOIN_FAILED | |
| SL_ZIGBEE_AF_ZLL_SENDING_DEVICE_INFORMATION_REQUEST_FAILED | |
| SL_ZIGBEE_AF_ZLL_SENDING_IDENTIFY_REQUEST_FAILED | |
| SL_ZIGBEE_AF_ZLL_SENDING_RESET_TO_FACTORY_NEW_REQUEST_FAILED | |
| SL_ZIGBEE_AF_ZLL_NETWORK_FORMATION_FAILED | |
| SL_ZIGBEE_AF_ZLL_NETWORK_UPDATE_OPERATION | |
sl_zigbee_af_image_block_request_options_t#
sl_zigbee_af_image_block_request_options_t
The list of options possible for the image block request/response.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE | |
| SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT | |
| SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER | |
| SL_ZIGBEE_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST | |
sl_zigbee_af_ota_storage_status_t#
sl_zigbee_af_ota_storage_status_t
Contain the success or error code of an OTA storage device operation.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_OTA_STORAGE_SUCCESS | |
| SL_ZIGBEE_AF_OTA_STORAGE_ERROR | |
| SL_ZIGBEE_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG | |
| SL_ZIGBEE_AF_OTA_STORAGE_PARTIAL_FILE_FOUND | |
| SL_ZIGBEE_AF_OTA_STORAGE_OPERATION_IN_PROGRESS | |
sl_zigbee_af_ota_download_result_t#
sl_zigbee_af_ota_download_result_t
Contain the success or error code of an OTA download operation.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS | |
| SL_ZIGBEE_AF_OTA_DOWNLOAD_TIME_OUT | |
| SL_ZIGBEE_AF_OTA_VERIFY_FAILED | |
| SL_ZIGBEE_AF_OTA_SERVER_ABORTED | |
| SL_ZIGBEE_AF_OTA_CLIENT_ABORTED | |
| SL_ZIGBEE_AF_OTA_ERASE_FAILED | |
sl_zigbee_af_key_establishment_notify_message_t#
sl_zigbee_af_key_establishment_notify_message_t
| Enumerator | |
|---|---|
| NO_APP_MESSAGE | |
| RECEIVED_PARTNER_CERTIFICATE | |
| GENERATING_EPHEMERAL_KEYS | |
| GENERATING_SHARED_SECRET | |
| KEY_GENERATION_DONE | |
| GENERATE_SHARED_SECRET_DONE | |
| LINK_KEY_ESTABLISHED | LINK_KEY_ESTABLISHED indicates Success, key establishment done. |
| NO_LOCAL_RESOURCES | Error codes: Transient failures where Key Establishment could be retried. |
| PARTNER_NO_RESOURCES | |
| TIMEOUT_OCCURRED | |
| INVALID_APP_COMMAND | |
| MESSAGE_SEND_FAILURE | |
| PARTNER_SENT_TERMINATE | |
| INVALID_PARTNER_MESSAGE | |
| PARTNER_SENT_DEFAULT_RESPONSE_ERROR | |
| BAD_CERTIFICATE_ISSUER | Fatal Errors: These results are not worth retrying because the outcome will not change. |
| KEY_CONFIRM_FAILURE | |
| BAD_KEY_ESTABLISHMENT_SUITE | |
| KEY_TABLE_FULL | |
| NO_ESTABLISHMENT_ALLOWED | Neither initiator nor responder is an ESP/TC so the key establishment is not allowed per the spec. |
| INVALID_CERTIFICATE_KEY_USAGE | |
sl_zigbee_af_image_verify_status_t#
sl_zigbee_af_image_verify_status_t
Indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer-specific verification.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_IMAGE_GOOD | |
| SL_ZIGBEE_AF_IMAGE_BAD | |
| SL_ZIGBEE_AF_IMAGE_VERIFY_IN_PROGRESS | |
sl_zigbee_af_cbke_key_establishment_suite_t#
sl_zigbee_af_cbke_key_establishment_suite_t
CBKE Library types.
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_INVALID_KEY_ESTABLISHMENT_SUITE | |
| SL_ZIGBEE_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1 | |
| SL_ZIGBEE_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1 | |
sl_zigbee_af_device_management_password_type_t#
sl_zigbee_af_device_management_password_type_t
| Enumerator | |
|---|---|
| UNUSED_PASSWORD | |
| SERVICE_PASSWORD | |
| CONSUMER_PASSWORD | |
sl_zigbee_af_device_management_change_pending_flags_t#
sl_zigbee_af_device_management_change_pending_flags_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK | |
| SL_ZIGBEE_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK | |
| SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK | |
| SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK | |
| SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK | |
| SL_ZIGBEE_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK | |
sl_zigbee_af_device_discovery_status_t#
sl_zigbee_af_device_discovery_status_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_NONE | |
| SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_NEW | |
| SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS | |
| SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS | |
| SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION | |
| SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_DONE | |
| SL_ZIGBEE_AF_DEVICE_DISCOVERY_STATUS_FAILED | |
Typedef Documentation#
sl_zigbee_af_profile_id_t#
typedef uint16_t sl_zigbee_af_profile_id_t
Refer to the Zigbee application profile ID.
sl_zigbee_af_attribute_id_t#
typedef uint16_t sl_zigbee_af_attribute_id_t
Refer to the ZCL attribute ID.
sl_zigbee_af_attribute_type_t#
typedef uint8_t sl_zigbee_af_attribute_type_t
Refer to the ZCL attribute type.
sl_zigbee_af_attribute_mask_t#
typedef uint8_t sl_zigbee_af_attribute_mask_t
User for the attribute mask.
sl_zigbee_af_generic_cluster_function_t#
typedef void(* sl_zigbee_af_generic_cluster_function_t) (void) )(void)
Use for either of the cluster functions.
This type is used for the array of the cluster functions and should always be cast into one of the specific functions before being called.
sl_zigbee_af_difference_type_t#
typedef uint64_t sl_zigbee_af_difference_type_t
Compare two ZCL attribute values. The size of this data type depends on the platform.
sl_zigbee_af_interpan_message_type_t#
typedef uint8_t sl_zigbee_af_interpan_message_type_t
Interpan Message type: unicast, broadcast, or multicast.
sl_zigbee_af_interpan_options_t#
typedef uint16_t sl_zigbee_af_interpan_options_t
The options for sending/receiving interpan messages.
sl_zigbee_af_allowed_interpan_options_t#
typedef uint8_t sl_zigbee_af_allowed_interpan_options_t
The options for what interpan messages are allowed.
sl_zigbee_af_tc_link_key_request_policy_t#
typedef sl_zigbee_tc_link_key_request_policy_t sl_zigbee_af_tc_link_key_request_policy_t
sl_zigbee_af_app_link_key_request_policy_t#
typedef sl_zigbee_app_link_key_request_policy_t sl_zigbee_af_app_link_key_request_policy_t
sl_zigbee_af_plugin_esi_management_bitmask_t#
typedef uint8_t sl_zigbee_af_plugin_esi_management_bitmask_t
Bitmask data type for storing one bit of information for each ESI in the ESI table.
sl_zigbee_af_service_discovery_callback_t#
typedef void() sl_zigbee_af_service_discovery_callback_t(const sl_zigbee_af_service_discovery_result_t *result) (const sl_zigbee_af_service_discovery_result_t *result)
Define a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, the callback is only fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast, multiple callbacks may be fired with SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a few seconds, the callback is fired with SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or SL_ZIGBEE_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.
sl_zigbee_af_partner_link_key_exchange_callback_t#
typedef void() sl_zigbee_af_partner_link_key_exchange_callback_t(bool success) (bool success)
Define a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.
sl_zigbee_af_network_event_handler_t#
typedef void(* sl_zigbee_af_network_event_handler_t) (void) )(void)
Refer to the handler for network events.
sl_zigbee_af_endpoint_event_handler_t#
typedef void(* sl_zigbee_af_endpoint_event_handler_t) (uint8_t endpoint) )(uint8_t endpoint)
Refer to the handler for endpoint events.
sl_zigbee_af_tick_function_t#
typedef void(* sl_zigbee_af_tick_function_t) (uint8_t endpoint) )(uint8_t endpoint)
Refer to the tick callback for cluster.
Tick function will be called once for each tick for each endpoint in the cluster. The rate of tick is determined by the metadata of the cluster.
sl_zigbee_af_init_function_t#
typedef void(* sl_zigbee_af_init_function_t) (uint8_t endpoint) )(uint8_t endpoint)
Refer to the init callback for cluster.
Init function is called when the application starts up, once for each cluster/endpoint combination.
sl_zigbee_af_cluster_attribute_changed_callback_t#
typedef void(* sl_zigbee_af_cluster_attribute_changed_callback_t) (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId) )(uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId)
Refer to the attribute changed callback function.
This function is called just after an attribute changes.
sl_zigbee_af_manufacturer_specific_cluster_attribute_changed_callback_t#
typedef void(* sl_zigbee_af_manufacturer_specific_cluster_attribute_changed_callback_t) (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, uint16_t manufacturerCode) )(uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, uint16_t manufacturerCode)
Refer to the manufacturer-specific attribute changed callback function.
This function is called just after a manufacturer-specific attribute changes.
sl_zigbee_af_cluster_pre_attribute_changed_callback_t#
typedef sl_zigbee_af_status_t(* sl_zigbee_af_cluster_pre_attribute_changed_callback_t) (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, sl_zigbee_af_attribute_type_t attributeType, uint8_t size, uint8_t *value) )(uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, sl_zigbee_af_attribute_type_t attributeType, uint8_t size, uint8_t *value)
Refer to the pre-attribute changed callback function.
This function is called before an attribute changes.
sl_zigbee_af_default_response_function_t#
typedef void(* sl_zigbee_af_default_response_function_t) (uint8_t endpoint, uint8_t commandId, sl_zigbee_af_status_t status) )(uint8_t endpoint, uint8_t commandId, sl_zigbee_af_status_t status)
Refer to the default response callback function.
This function is called when default response is received, before the global callback. Global callback is called immediately afterwards.
sl_zigbee_af_message_sent_function_t#
typedef void(* sl_zigbee_af_message_sent_function_t) (sl_zigbee_outgoing_message_type_t type, uint16_t indexOrDestination, sl_zigbee_aps_frame_t *apsFrame, uint16_t msgLen, uint8_t *message, sl_status_t status) )(sl_zigbee_outgoing_message_type_t type, uint16_t indexOrDestination, sl_zigbee_aps_frame_t *apsFrame, uint16_t msgLen, uint8_t *message, sl_status_t status)
Refer to the message sent callback function.
This function is called when a message is sent.
sl_zigbee_af_remote_cluster_type_t#
typedef uint16_t sl_zigbee_af_remote_cluster_type_t
Zigbee Internet Client/Server Remote Cluster Types.
sl_zigbee_af_zcl_request_status_t#
typedef uint32_t sl_zigbee_af_zcl_request_status_t
return status for cluster request handlers - may be `sl_zigbee_af_status_t` or a special return status indicate special handling of the response by the request handler