Keep track of cluster-related events and their sleep control values. The cluster code will not know at runtime all of the events that it has access to in the event table This structure is stored by the application framework in an event context table which along with helper functions allows the cluster code to schedule and deactivate its associated events.
Public Attribute Documentation#
clusterId#
sl_zigbee_af_cluster_id_t sl_zigbee_event_context_t::clusterId
The cluster ID of the associated cluster event.
isClient#
bool sl_zigbee_event_context_t::isClient
The server/client identity of the associated cluster event.
pollControl#
sl_zigbee_af_event_poll_control_t sl_zigbee_event_context_t::pollControl
A poll control value used to control the network polling behavior while the event is active.
sleepControl#
sl_zigbee_af_event_sleep_control_t sl_zigbee_event_context_t::sleepControl
A sleep control value used to control the processor's sleep behavior while the event is active.
event#
sli_zigbee_event_t* sl_zigbee_event_context_t::event
A pointer to the event control value which is stored in the event table and is used to actually schedule the event.