Describe clusters that are on the endpoint.

Public Attribute Documentation#

cluster#

sl_zigbee_af_cluster_t* sl_zigbee_af_endpoint_type_t::cluster

Pointer to the cluster structs, describing clusters on this endpoint type.


clusterCount#

uint8_t sl_zigbee_af_endpoint_type_t::clusterCount

Number of clusters in this endpoint type.


endpointSize#

uint16_t sl_zigbee_af_endpoint_type_t::endpointSize

Size of all non-external, non-singlet attribute, in this endpoint type.