You are viewing documentation for version:
Use for all trust center backup data.
The 'keyList' pointer must point to an array and 'maxKeyListLength' must be populated with the maximum number of entries the array can hold.
Functions that modify this data structure will populate 'keyListLength' indicating how many keys were actually written into 'keyList'.
Public Attribute Documentation#
extendedPanId#
sl_802154_long_addr_t sl_zigbee_af_trust_center_backup_data_t::extendedPanId
keyListLength#
uint8_t sl_zigbee_af_trust_center_backup_data_t::keyListLength
maxKeyListLength#
uint8_t sl_zigbee_af_trust_center_backup_data_t::maxKeyListLength
keyList#
sl_zigbee_af_link_key_backup_data_t* sl_zigbee_af_trust_center_backup_data_t::keyList