Map actual endpoint type onto a specific endpoint.
Public Attribute Documentation#
profileId#
sl_zigbee_af_profile_id_t sl_zigbee_af_defined_endpoint_t::profileId
Profile ID of the device on this endpoint.
deviceId#
uint16_t sl_zigbee_af_defined_endpoint_t::deviceId
Device ID of the device on this endpoint.
endpointType#
sl_zigbee_af_endpoint_type_t* sl_zigbee_af_defined_endpoint_t::endpointType
Endpoint type for this endpoint.
bitmask#
sl_zigbee_af_endpoint_bitmask_t sl_zigbee_af_defined_endpoint_t::bitmask
Meta-data about the endpoint.