Describe the attribute default, min, and max values.
This struct is required if the attribute mask specifies that this attribute has a known min and max values.
Public Attributes#
Public Attribute Documentation#
defaultValue#
sl_zigbee_af_default_attribute_value_t sl_zigbee_af_attribute_min_max_value_t::defaultValue
Default value of the attribute.
minValue#
sl_zigbee_af_default_attribute_value_t sl_zigbee_af_attribute_min_max_value_t::minValue
Minimum allowed value.
maxValue#
sl_zigbee_af_default_attribute_value_t sl_zigbee_af_attribute_min_max_value_t::maxValue
Maximum allowed value.