sl_bt_evt_advertiser_timeoutAdvertiser#
Indicates the advertising of an advertising set has stopped, because the advertiser has completed the configured number of advertising events or the advertising has reached the configured duration.
Data Structures#
struct | sl_bt_evt_advertiser_timeout_s Data structure of the timeout event. |
Macros#
#define | sl_bt_evt_advertiser_timeout_id 0x010400a0 Identifier of the timeout event. |
Detailed Description#
Indicates the advertising of an advertising set has stopped, because the advertiser has completed the configured number of advertising events or the advertising has reached the configured duration.
The maximum number of advertising events or advertising duration can be configured by the maxevents or duration parameter in the command sl_bt_advertiser_set_timing.
Data Structure Documentation#
sl_bt_evt_advertiser_timeout_s#
struct sl_bt_evt_advertiser_timeout_s
Data structure of the timeout event.
Data Fields | ||
|---|---|---|
uint8_t | handle | The advertising set handle |