sl_bt_evt_test_dtm_completedTesting Commands#
Indicates that the radio has processed a test start or end command.
Data Structures | |
struct | |
Data structure of the dtm_completed event. | |
Macros | |
# define | sl_bt_evt_test_dtm_completed_id 0x000e00a0 |
Identifier of the dtm_completed event. | |
Detailed Description#
Indicates that the radio has processed a test start or end command.
The result parameter indicates the success of the command.
After the receiver or transmitter test is stopped, the number_of_packets parameter in this event indicates the number of received or transmitted packets.
Data Structure Documentation#
sl_bt_evt_test_dtm_completed_s#
struct sl_bt_evt_test_dtm_completed_s |
Data structure of the dtm_completed event.
Data Fields | |
|---|---|
uint16_t | |
result | Command result |
uint16_t | |
number_of_packets | Number of packets |
Only valid for sl_bt_test_dtm_end command. |