sl_bt_evt_gatt_server_attribute_valueGATT Server#
Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.
Data Structures#
struct | sl_bt_evt_gatt_server_attribute_value_s Data structure of the attribute_value event. |
Macros#
#define | sl_bt_evt_gatt_server_attribute_value_id 0x000a00a0 Identifier of the attribute_value event. |
Detailed Description#
Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.
The parameter att_opcode describes which GATT procedure was used to change the value.
Data Structure Documentation#
sl_bt_evt_gatt_server_attribute_value_s#
struct sl_bt_evt_gatt_server_attribute_value_s
Data structure of the attribute_value event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint16_t | attribute | Attribute Handle |
uint8_t | att_opcode | Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received. |
uint16_t | offset | Value offset |
value | Value | |