sl_bt_evt_connection_rssiConnection#
Triggered when an connection_get_rssi command has completed.
Data Structures#
struct | Data structure of the rssi event. |
Macros#
#define | sl_bt_evt_connection_rssi_id 0x030600a0 Identifier of the rssi event. |
Detailed Description#
Triggered when an connection_get_rssi command has completed.
Data Structure Documentation#
sl_bt_evt_connection_rssi_s#
struct sl_bt_evt_connection_rssi_s
Data structure of the rssi event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint8_t | status | Command complete status:
|
int8_t | rssi | The median of the last seven measured RSSI values on the connection. Units: dBm. Range: -127 to +20. Ignore this parameter if the command fails. |