sl_bt_evt_dfu_boot_failureDevice Firmware Update#
This event indicates that an error, which prevents the device from booting, has occurred in bootloader.
Data Structures#
struct | Data structure of the boot_failure event. |
Macros#
# define | sl_bt_evt_dfu_boot_failure_id 0x010000a0 Identifier of the boot_failure event. |
Detailed Description#
This event indicates that an error, which prevents the device from booting, has occurred in bootloader.
Data Structure Documentation#
sl_bt_evt_dfu_boot_failure_s#
struct sl_bt_evt_dfu_boot_failure_s
Data structure of the boot_failure event.
Data Fields | ||
|---|---|---|
uint16_t | reason | The reason for boot failure. |